|
NXP NFC Reader Library
v4.040.05.011646
|
T4T parameter structure. More...
Data Fields | |
| void * | pAlT4TDataParams |
| Pointer to T4T data parameters. | |
| uint8_t | aNdefFileID [2] |
| NDEF File ID to Create. | |
| uint8_t | bRa |
| NDEF file read access condition size. | |
| uint8_t | bWa |
| NDEF file write access condition size. | |
| uint8_t | bCurrentSelectedFile |
| Current selected file. | |
| uint16_t | wMLe |
| MLe supported by card (obtained from CC) | |
| uint16_t | wMLc |
| MLc supported by card (obtained from CC) | |
| uint16_t | wCCLEN |
| Size of CCr,Valid CCLEN range 000Fh-FFFEh. More... | |
| uint16_t | wMaxFileSize |
| Maximum NDEF file size in bytes. | |
T4T parameter structure.
| uint16_t phalTop_T4T::wCCLEN |
Size of CCr,Valid CCLEN range 000Fh-FFFEh.