These Components configure PHPAL_I14443P4A.
More...
|
| phStatus_t | phpalI14443p4a_Rats (void *pDataParams, uint8_t bFsdi, uint8_t bCid, uint8_t *pAts) |
| | Perform a ISO14443-4A "Request Answer to Select" command. More...
|
| |
| phStatus_t | phpalI14443p4a_Pps (void *pDataParams, uint8_t bDri, uint8_t bDsi) |
| | Perform a ISO14443-4A "Protocol and Parameter Selection" command. More...
|
| |
| phStatus_t | phpalI14443p4a_ActivateCard (void *pDataParams, uint8_t bFsdi, uint8_t bCid, uint8_t bDri, uint8_t bDsi, uint8_t *pAts) |
| | Perform ISO14443-4A Rats and Pps commands. More...
|
| |
| phStatus_t | phpalI14443p4a_GetProtocolParams (void *pDataParams, uint8_t *pCidEnabled, uint8_t *pCid, uint8_t *pNadSupported, uint8_t *pFwi, uint8_t *pFsdi, uint8_t *pFsci) |
| | Retrieve the ISO14443-4A protocol parameters. More...
|
| |
| phStatus_t | phpalI14443p4a_SetConfig (void *pDataParams, uint16_t wConfig, uint16_t wValue) |
| | Set configuration parameter. More...
|
| |
These Components configure PHPAL_I14443P4A.
These Components implement the additional ISO/IEC 14443-4 activation steps needed for ISO14443 Type-A cards.
§ PHPAL_I14443P4A_CONFIG_OPE_MODE
| #define PHPAL_I14443P4A_CONFIG_OPE_MODE 0x01 |
§ PHPAL_I14443P4A_CONFIG_RATS_RETRY_COUNT
| #define PHPAL_I14443P4A_CONFIG_RATS_RETRY_COUNT 0x02 |
§ PHPAL_I14443P4A_DATARATE_106
| #define PHPAL_I14443P4A_DATARATE_106 0x00U |
DRI/DSI value for 106 kBit/s.
§ PHPAL_I14443P4A_DATARATE_212
| #define PHPAL_I14443P4A_DATARATE_212 0x01U |
DRI/DSI value for 212 kBit/s.
§ PHPAL_I14443P4A_DATARATE_424
| #define PHPAL_I14443P4A_DATARATE_424 0x02U |
DRI/DSI value for 424 kBit/s.
§ PHPAL_I14443P4A_DATARATE_848
| #define PHPAL_I14443P4A_DATARATE_848 0x03U |
DRI/DSI value for 848 kBit/s.
§ PHPAL_I14443P4A_RATS_RETRY_MAX
| #define PHPAL_I14443P4A_RATS_RETRY_MAX 1 |
Maximum retry value of RATS during transmission and timeout error.
§ PHPAL_I14443P4A_RATS_RETRY_MIN
| #define PHPAL_I14443P4A_RATS_RETRY_MIN 0 |
Minimum retry value of RATS during transmission and timeout error.
§ phpalI14443p4a_Rats()
Perform a ISO14443-4A "Request Answer to Select" command.
[FSDI to FSD conversion]
---------------------------------------------------------------
FSDI | 00 | 01 | 02 | 03 | 04 | 05 | 06 | 07 | 08 |
---------------------------------------------------------------
FSD (bytes) | 16 | 24 | 32 | 40 | 48 | 64 | 96 | 128 | 256 |
---------------------------------------------------------------
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | bFsdi | Frame Size Integer; 0-8. |
| [in] | bCid | Card Identifier; 0-14. |
| [out] | pAts | Answer to Select; uint8_t[255]. |
§ phpalI14443p4a_Pps()
| phStatus_t phpalI14443p4a_Pps |
( |
void * |
pDataParams, |
|
|
uint8_t |
bDri, |
|
|
uint8_t |
bDsi |
|
) |
| |
Perform a ISO14443-4A "Protocol and Parameter Selection" command.
The following values for bDri and bDsi are possible:
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | bDri | Divisor Receive (PCD to PICC) Integer; 0-3. |
| [in] | bDsi | Divisor Send (PICC to PCD) Integer; 0-3. |
§ phpalI14443p4a_ActivateCard()
Perform ISO14443-4A Rats and Pps commands.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | bFsdi | Frame Size Integer; 0-8. |
| [in] | bCid | Card Identifier; 0-14. |
| [in] | bDri | Divisor Receive (PCD to PICC) Integer; 0-3. |
| [in] | bDsi | Divisor Send (PICC to PCD) Integer; 0-3. |
| [out] | pAts | Answer to Select; uint8_t[255]. |
§ phpalI14443p4a_GetProtocolParams()
Retrieve the ISO14443-4A protocol parameters.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [out] | pCidEnabled | Unequal '0' if Card Identifier is enabled. |
| [out] | pCid | Card Identifier. |
| [out] | pNadSupported | Node Address Support; Unequal '0' if supported. |
| [out] | pFwi | Frame Waiting Integer. |
| [out] | pFsdi | PCD Frame Size Integer; 0-8. |
| [out] | pFsci | PICC Frame Size Integer; 0-8. |
§ phpalI14443p4a_SetConfig()
| phStatus_t phpalI14443p4a_SetConfig |
( |
void * |
pDataParams, |
|
|
uint16_t |
wConfig, |
|
|
uint16_t |
wValue |
|
) |
| |
Set configuration parameter.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | Pointer to this layers parameter structure. |
| [in] | wConfig | Configuration Identifier. |
| [in] | wValue | Configuration Value. |