| Freescale Semiconductor | |||||||||||||
| RSA Example Application for 56F82x | |||||||||||||
| Overview | |||||||||||||
| The demo is based on File I/O. The file m.in is used to store message words for RSA. After encryption, the | |||||||||||||
| coded message is stored in m_Enc.out; after decryption, the decoded message is stored in m_Dec.out. The | |||||||||||||
| contents of m_Dec.out must be the same as that of m.in. The contents of the input file (i.e., the message) | |||||||||||||
| could be text, numbers and/or special characters. | |||||||||||||
| How to get this software | |||||||||||||
| This example application is included as part of the CodeWarrior Development Studio for 56800/E Digital | |||||||||||||
| Signal Controllers. Follow these steps: | |||||||||||||
| 1. | Install CodeWarrior Development Studio for 56800/E Digital Signal Controllers | ||||||||||||
| 2. | Launch CodeWarrior, and create new Processor Expert project | ||||||||||||
| a. | Select File > New menu | ||||||||||||
| b. | Select Processor Expert Examples Stationery | ||||||||||||
| c. | Type project name | ||||||||||||
| d. | Click OK | ||||||||||||
| e. | Select DemoApplications > Security > RSA > 56f827 | ||||||||||||
| f. | Click OK | ||||||||||||
| 3. | Generate application code by selecting Processor Expert > Generate Code menu | ||||||||||||
| Detailed documentation | |||||||||||||
| Documentation for this application is included as part of this example project. Expand Doc folder located | |||||||||||||
| in the project window by clicking on the + icon next to the folder, and open desired file by double clicking it. | |||||||||||||
| Freescale™ and the Freescale logo are trademarks of Freescale Semiconductor, Inc. All other product | |||||||||||||
| or service names are the property of their respective owners. | |||||||||||||
| ©2005, Freescale Semiconductor, Inc | |||||||||||||