Freescale Semiconductor
VRLite-1 Example Application for 56F82x
Overview
The VRLite-1 library provides two demos:
  demo_vrlite1 allows the user to train and recognize the following words in real time:
Answer, AreaCode, Book, Call, Cancel, ChargeCard, CreditCard, Dial Operator, Eight Hundred, 
Emergency, End, Friend, Home, Information, Office, Public Directory, Secretary, Security, Stop Demo
These words have been chosen to illustrate the capability of the VRLite-1 library in cell phone
applications.
  demo_dial_vrlite1 allows the user to train and recognize words in real time and dial the number using
PE’s DTMF Generation library.
For example, suppose the user trains the word Dial Operator. Once the user recognizes this word, the
demo dials the number stored in an array that corresponds to the Operator
How to get this software
This example application is included as part of the CodeWarrior Development Studio for 56800/E Digital
Signal Controllers. Follow these steps:
1. Install CodeWarrior Development Studio for 56800/E Digital Signal Controllers
2. Launch CodeWarrior, and create new Processor Expert project
a. Select File > New menu
b. Select Processor Expert Examples Stationery
c. Type project name
d. Click OK
e. Select DemoApplications > Speech > vr_lite1 > 56F827
f. Click OK
3. Generate application code by selecting Processor Expert > Generate Code menu
Detailed documentation
Documentation for this application is included as part of this example project. Expand Doc folder located
in the project window by clicking on the + icon next to the folder, and open desired file by double clicking it.
Freescale™ and the Freescale logo are trademarks of Freescale Semiconductor, Inc. All other product
or service names are the property of their respective owners. 
©2005, Freescale Semiconductor, Inc