Finalization of halogen-free transfer
Small-signal discrete and logic SMD plastic packages go “Dark Green”
As one of the first suppliers in the market, NXP now finalizes the transfer to halogen-free packaging technology for its small-signal discrete and logic surface mount devices (SMD). From now on the majority of discretes and logic produced ban the use of halogens and antimony in the material, which is used as flame retardant in the mold compound. Additionally, Dark Green products are also fully RoHS compliant with the European Union directive 2002/95/EC. At the same time, the shift to halogen-free does not change any product parameters nor affect existing qualification, such as the automotive standard AEC-Q101 that some products are compliant with.
NXP Dark Green products do not contain the substances exceeding the limits as below:
| Substances | Limit |
| Antimony Oxides (Sb2O3, Sb2O5) | < 900 ppm |
| Chlorinated + Brominated Compounds | Σ < 900 ppm |
NXP customers benefit from this transfer to Dark Green as environmental safety aspects are getting more important for manufacturing processes and are acknowledged as a value of its own in the eyes of end customers.
Years ahead of upcoming legislation, NXP has already developed products in packages such as its ultra-small discrete leadless and Logic leadless DQFN and MicroPak that are exclusively assembled in Dark Green mold compound since inception. These activities reflect NXP's deep commitment to developing eco-friendly products and integrating environmental safety aspects in all manufacturing processes. “Dark Green” products can be recognized by the “Halogen Free” logo on the box label.
Discrete / Logic SMD plastic packages - Dark Green transfer finalised |
| Package | Package description |
| SOD123F | SMD package, 2 pins |
| SOD123W | SMD package "FlatPower", 2 pins |
| SOD128 | SMD package "FlatPower", 2 pins |
| SOD323 (SC-76) | SMD package, 2 pins |
| SOD323F (SC-90) | SMD package, 2 pins |
| SOD523 (SC-79) | SMD package, 2 pins |
| SOD882 | Leadless ultra small package, 2 terminals |
| SOT1045 | Leadless DQFN, 20 terminals |
| SOT1059 (XSON10U) | Leadless ultra-thin package, 10 terminals |
| SOT1061 (HUSON3) | Leadless package, 3 terminals |
| SOT1089 | Leadless package, 3 terminals |
| SOT1115 | Leadless MicroPak, 8 terminals |
| SOT1116 | Leadless MicroPak, 6 terminals |
| Leadless MicroPak, 60 terminals | |
| SOT143B | SMD package, 4 pins |
| SOT223 (SC-73) | SMD package, 4 pins |
| SOT23 | SMD package, 3 pins |
| SOT323 (SC-70) | SMD package, 3 pins |
| SOT353 (SC-88A) | PicoGate / SMD package, 5 pins |
| SOT362 | TSSOP, 48 pins |
| SOT363 (SC-88) | PicoGate / SMD package, 6 pins |
| SOT416 (SC-75) | SMD package, 3 pins |
| SOT457 (SC-74) | PicoGate / SMD package, 6 pins |
| SOT505-2 | PicoGate, 8 pins |
| SOT536 | BGA, 96 balls |
| SOT537 | BGA, 114 balls |
| SOT650 | Leadless MicroPak, 10 terminals |
| SOT663 | SMD package, 3 pins |
| SOT665 | SMD package, 5 pins |
| SOT666 | SMD package, 6 pins |
| SOT702 | BGA, 56 balls |
| SOT753 | PicoGate, 5 pins |
| SOT762 | Leadless DQFN, 14 terminals |
| SOT763 | Leadless DQFN, 16 terminals |
| SOT764 | Leadless DQFN, 20 terminals |
| SOT815 | Leadless DQFN, 24 terminals |
| SOT833 | Leadless ultra small package / MicroPak, 8 terminals |
| SOT883 (SC-101) | Leadless ultra small package / MicroPak, 3 terminals |
| SOT886 (XSON6) | Leadless ultra small package / MicroPak, 6 terminals |
| SOT891 (XSON6) | Leadless ultra small package / MicroPak, 6 terminals |
| SOT902 | Leadless MicroPak, 8 terminals |
| SOT996 | PicoGate, 8 pins |
Discrete / Logic SMD plastic packages - Dark Green transfer schedule |
| Package | Package description | Dark Green transfer |
| SOT89 (SC-62) | SMD package, 3 pins | Transfer in Q1 2010 |
| SOT108 | SO Packages, 14 pins | Transfer in Q1 2010 |
| SOT109 | SO Packages, 16 pins | Transfer in Q1 2010 |
| SOT163 | SO Packages, 20 pins | Transfer in Q1 2010 |
| SOT137 | SO Packages, 24 pins | Transfer in Q1 2010 |
| SOT402 | TSSOP, 14 pins | Transfer in Q4 2009 |
| SOT403 | TSSOP, 16 pins | Transfer in Q4 2009 |
| SOT360 | TSSOP, 20 pins | Transfer in Q4 2009 |
| SOT355 | TSSOP, 24 pins | Transfer in Q4 2009 |
Regular updates
To keep current with our latest announcements, be sure to sign up for eNews, our customizable electronic newsletter that saves you time by sending you only the information you want.