Select site:
English
Campus Innovator’s Challenge winners!


NXP Campus

Design the next must-have product - that was NXP Semiconductors challenge to electronic and engineering students in mainland China. At a special ceremony in Shanghai on November 28, winners of the first NXP campus Innovator's Challenge received their design awards.


Launched in April earlier this year, the competition attracted 544 team registrations from more than 110 universities and colleges across China. All that was needed to enter our campus Innovator's Challenge competition was for students to develop an innovative idea into an application circuit board using NXP products. To help the students get started we gave a NXP's 32-bit LPC2xxx ARM microcontroller development board together with some of our recommended key interface products.


232 design proposals were submitted during the initial round. From these, 50 were selected to enter the second round and finally, on November 6, the top ten teams were chosen for a final demonstration held on November 27.


Awards

Design project Brief Winner's university Design team members:
Design of a Miniature Urine Analyzer Based on Embedded System

This is a house use Miniature Urine Analyzer based on Embedded System. The high density microcontroller LPC2148 developed by NXP company is adopted. USB controller integrated inside the chips is responsible for power supplying and data transmission. The integrated ADC inside processor can acquire the analog signal output by CCD, while the SPI interface inside sets up communication bridges of touch-screen module and Ethernet module. The touch screen is used in all process of operation and it also have friendly interface during the operation. The design of photoelectric detected system not only get rid of the error caused by mechanism transmission of traditional instrument, but also reduce the size and the consume of energy.

Chongqing University , Chongqing

  • Teng Ma
  • Yingming You
  • Yong Liu
  • Xin Wang
High-performance Balance Charger for Power Li-Po Battery

A powerful Li-Po balance charger based on LPC2148 is designed in this project. Taking full advantages of ARM resources, the charger provides sound management for the battery charge-discharge function. It can support 1S to 6S Li-Po battery balance charging. Release current and voltage are adjustable for each piece of battery. The charger monitors and displays the health status, capacity, internal resistance and other information of each monomer in Real-time. It can also upload information to PC, which is easy for analysis and management. To ensure independent and reliable charging for each monomer, a six-channel Isolation DC-DC Converter System was designed independently. Humanized design facilitates the maintenance of battery and reduces security risks. It is an ideal choice for battery maintaining of the electrical equipment, model airplane and military drone.

BeiHang University (Beijing University of Aeronautics & Astronautics)

  • Chao Han
  • Shichao Zhang
  • Zhun Miao
A super marker crash machine based on LAN,RFID&Finger Printer Recognition Technologies

The system constitutes a TCP-based LAN by making full use of the NXP high performance processor LPC2378; and it utilizes the advanced RFID label-sampling technique to quickly, effectively and safely sample the commodity labels; at the same time, the finger print recognizing technique enables the membership management, the fingerprint account system. At the client, the uCOS+uCTCP/IP+ZLG/GUI structure is used, while at the server, the SQL database is used as the high performance server. Innovative ideas plus ingenious design enables a wonderful and passionate experience when shopping, and speed up your life…

South China University of Technology

  • Hanyu Yan
  • Zhenghua Kang
  • Mengdan Zou
  • Zhibin Huang
Real-Time Positioning System for Automobiles

This system is designed to provide a means to enable the user to use a cellphone to communicate with the far-end subsystem to obtain the required information about the automobile. It operates in one of two modes: for alarm mode, the far-end sends an alarm message to the user when the automobile moves without prior permission. For normal mode, the user can send instructions to the far-end to obtain information such as position and velocity, as well as to control the operation of the automobile.

Tsinghua University

  • Mingcheng Ni
  • Yuanlu Xie
  • Lei Wang
Development of Bioelectrical Impedance Analyzer

Bio-impedance technology is a noninvasive detecting method which utilize the characters of tissue (impedance/admittance) and its variation to detect human body related biomedical information. This program is aimed to develop a mini digital bio-impedance analyzer. The analyzer equips an LPC2148 MCU as its main controller, and communicate with the PC via USB connection. It parse the instruction from PC, complete the multi-frequency complex impedance measurement and upload the data to PC. These results can be applied to the analysis of human body composition such as body fat percent, body weight without fat and so on.

Nanjing University

  • Chengyu Huo
  • Xiaoliang Ji
  • Songxin Huan
  • Rong Zhang
Wireless Automatic Meter Reading System

There are some problems existing in the traditional manual meter-reading manner, such as entering residents' house difficultly, low efficiency, making mistakes easily and so on. In order to solve these problems, a new project is brought forward, which is the Wireless Automatic Meter Reading System. Building Collector, the core part of the system, is constructed with LPC2148 and other peripherals such as RS-232, Infrared, Wireless and FRAM circuit. Community Collector, the background part of the system, consists of PC and bidirectional wireless communication modules. The Building Collector receives water meter data in fixed time or fixed amount. According to the customized protocol between the Community Collector and the Building Collector, the system implements meter reading, time checking and other functions. Collecting data without wire, multiple meter reading manners and convenient for installation and maintenance are the three main features of the system.

Nanjing University of Aeronautics and Astronautics

  • Zhongye Zheng
  • Shugang Xie
  • Hui Wang
  • Yanbing Bai
Wireless Data Acquiring System based on LPC2378

The project mainly designed and implemented a Distributed Self-Organization Wireless Data Acquiring System, which consists of one main node and several sub-nodes. The main node realized functions of Ethernet communication, wireless communication, display, storage and thermal protect, etc. Major functions of sub- node are wireless communication and data acquiring.

Nanjing University of Aeronautics and Astronautics

  • Lin Chen
  • Dezhi Zeng
  • Yunfeng Zai
  • Qinyu Wang
Intelligent output power elevator conditioning system based on the PWM

This design mainly inducts motor drive and control, the essence of which is a small power converter, it simulates the load on the escalator by adjustable resistance, the control system changing with the load adjusts the motor rate of the output power , and it can adjust the asynchronous motor rate of the output power by constant pressure and frequency control method ,so it can play the role of energy-saving.Its advantages and innovations come as follows :

  1. Using full-bridge rectifier inverter technology;
  2. To save more energy by constant pressure and frequency control method ;
  3. Overload Protection Alarm;
  4. Costs lower than other frequency converters;
  5. Has some certain value of popularization.

South China Agricultural University

  • Zhihao Mo
  • Yongjiang Murong
  • Fuquan Luo
  • Zhibiao Huang
A Positioning Sensorless Universal Controller of BLDC Motors

The application mainly achieves adjustment of speed by way of controlling switches on IPM with LPC2148.The signal which can variate speed can be confirmed by a rheostat .The A/D interface on MCU captures the signal and calculates the time and PWM duty ratio and then adjusts the speed of BLDC motor. The red switch on the board can change the turning of the motor instantly.

Shenyang University for Technology

  • Dianhai Zhang
  • Yunlong Xu
Electronic Ticketing Management System based on RFID

The system is based on μc/OS embedded system technologies. By fully using LPC2148FBD64 microprocessor controller and MC RF500 RFID chip, the system (Wireless+ RFID combined system) could provide users with fast, flexible and mobile tag identification service (handheld reader) by making use of wireless transmission and touching-screen operation feature. Due to central database, network tickets sales and real-time tickets inspection extraordinarily enhance ticketing efficiency. Compared with the traditional ticketing management system, this system has many advantages, such as recycled, high-level security, non-touching operation and high speed identification and easily extended statistics collection. When properly adapted, this system increases the convenience in ticketing services, hence enhancing the value of overall services which can be marketed to beyond the scope of ticketing services.

Huazhong University of Science and Technology

  • Chuanbing Xiang
  • Xi Chen
  • Jie Huang
  • Ming Hu

Winning ways

The challenge competition forms part of NXP Semiconductors' long-term support programme for China's university talent development. Associated with the competition, a series of campus seminars were held in universities across the country, introducing our microcontroller and interface products knowledge to hundreds of students. Online web seminars were also hosted, with more than one thousand registrations. In addition, a bulletin board system was set up as a student forum for discussions and to provide them with prompt technical help from experts.


Regular updates

To keep current with our latest announcements, be sure to sign up for eNews, our customizable electronic newsletter that saves you time by sending you only the information you want.