FSL-UT-CAN-002
~~~~~~~~~~~~~~~

[cols=">s,6a",frame="topbot",options="header"]
|====================================================================
|Name | Description

| Summary |
CAN wakeup

| Automated |
No

| Kernel Config Option |

| Software Dependency |
N/A

| Non-default Hardware Configuration |
N/A

| Test Procedure |

Note: The CAN self-wakeup function is enabled by default.

. Active CAN interface

  ip link set can0 up type can bitrate 125000

. Enter Low power mode

  echo mem > /sys/power/state

. Tie CAN's Tx to GND to wakeup the systerm.

  Alternatively user can use another CAN to send frames to the sleep can to wakeup it.

| Expected Result |
Those operations should be successful.

|====================================================================

<<<