FSL-UT-CAN-003
~~~~~~~~~~~~~~~

[cols=">s,6a",frame="topbot",options="header"]
|====================================================================
|Name | Description

| Summary |
CAN send message

| Automated |
No

| Kernel Config Option |

| Software Dependency |
N/A

| Non-default Hardware Configuration |
N/A

| Test Procedure |

.Note
. If there's no KVASER CAN, can protocal analyzer, user can use
procedure B for test.

. For kernel earlier than 2.6.38, user still needs use the old way as
before to test can.

.Procedure A

. Connect CAN interface(can0) on board with KVASER CAN

. Active CAN interface

  ip link set can0 up type can bitrate 125000

. Run cansend to transmit one message.

  cantest can0 1F334455#1122334455667788

. Check the data that KVASER CAN recieved.

.Procedure B
. Get a FlexCAN loop-back connector or cable lines and connect it between CAN1 and CAN2.

. Active CAN interface

  ip link set can0 up type can bitrate 125000

  ip link set can1 up type can bitrate 125000

. Put can0 into receive mode in a background process

  cantest can0&

. Send test packet from CAN1 to CAN0

  cantest can1 1F334455#1122334455667788

| Expected Result |
The can0 should print the received frame 1F334455#1122334455667788
from can1.

|====================================================================

<<<