FSL-UT-GPU-001
~~~~~~~~~~~~~~~

[cols=">s,6a",frame="topbot",options="header"]
|====================================================================
|Name | Description

| Summary |
GPU function test

- tutorial3: test OpenGL ES 1.1 basic function
- tutorial4_es20: test OpenGL ES 2.0 basic function
- tiger: test OpenVG 1.1 basic function
- tvui: test Raster 2D and LibVivanteDK API

| Automated |
NO

| Kernel Config Option |
CONFIG_MXC_GPU_VIV=y

| Software Dependency |
N/A

| Non-default Hardware Configuration |
LVDS Display Panel

| Test Procedure |
. run the following command on target board,

 $ /unit_tests/gpu.sh

| Expected Result |
Should get the following message:

The frames can be drawn properly on screen

- tutorial3: a cube with texture rotating in the middle of the screen.
- tutorial4_es20: draws a glass sphere inside a big sphere (enviroment mapping). The glass sphere shows both reflection and refraction effects.
- tiger: a tiger spinning on the screen.
- tvui: draws several movie clips and a tv control panel.

|====================================================================

<<<