FSL-UT-NAND-001
~~~~~~~~~~~~~~~

[cols=">s,6a",frame="topbot",options="header"]
|====================================================================
|Name | Description

| Summary |
NAND TEST

| Automated |
No

| Kernel Config Option |

| Software Dependency |
N/A

| Non-default Hardware Configuration |
N/A

| Test Procedure |
After the system boots up with the NAND MTD driver,
it may be tested as follows (note that mtd-utils package is needed):

UBIFS :
add the following to kernel parameter line when it boots:
    "mtdparts=gpmi-nfc:20m(boot),200m(test),-(user)"
Find out the available partition(s) in the running Linux system.
So user can opt to test partition after this. For example:

   root@freescale ~$ cat /proc/mtd
   dev:  size   erasesize  name
   mtd0: 00140000 00020000 "boot"
   mtd1: 00140000 00020000 "test"
   mtd2: 0001f000 00008000 "user"

Erase one of the NAND Flash partitions using flash_eraseall.
Take /dev/mtd2 for example:

  $flash_eraseall /dev/mtd2

Create a ubi node:

  $ubiattach /dev/ubi_ctrl -m 2

create a ubi partition in this ubi node:

 $ubimkvol /dev/ubi0 -N testnode -m

Mount the NAND partition and read the files:

 $mkdir -p /tmp/mtdX
 $mount -t ubifs ubi0:testnode /tmp/mtdX
 $bonnie++ -d /tmp/mtdX -u 0 -s 2 -r 1
 $umount /tmp/mtdX
 $ubidettach /dev/ubi_ctrl -m 2

| Expected Result |
Those operations should be successful.

|====================================================================

<<<