These files are for convinience for secure boot testers

File Description
------------------------------------
"gen_fuse" :
	This script should be copied to "BLN_CST_MAIN_01.00.00/crts" and
        run to generate SRK footprint file "SRK_1_2_3_4_fuse.bin"
	The footprint value is also dumped out, they should be written to
	SRK fuse later

"u-boot/mk_secure_uboot"
"uImage/mk_secure_uimage"
"templates/"
	Automatic secure uboot and uImage generation scripts. These files
	are used for dynamic authentication. It is more convinient and
	adaptive comparing to the original static way.

	Copy "u-boot/mk_secure_uboot" to "BLN_CST_MAIN_01.00.00/u-boot"
	Copy "uImage/mk_secure_uimage" to "BLN_CST_MAIN_01.00.00/uImage"
	Copy "templates/" to "BLN_CST_MAIN_01.00.00"

Secure Boot Genreation
------------------------------------
For generating secure uboot
    . copy "u-boot.bin" to "BLN_CST_MAIN_01.00.00/u-boot"
    . "./mk_secure_uboot 0x87800000"
	- where 0x87800000 is the DDR location where u-boot is
	  copied to by ROM code, different from platform to platform
    . u-boot-signed-pad.bin will be generated. It is the u-boot image
      with signature

For generating secure uImage
    . copy "uImage" to "BLN_CST_MAIN_01.00.00/uImage"
    . "./mk_secure_uimage 0x80800000"
	- where 0x80800000 is the DDR location where uImage is
	  copied to by UBoot, different from platform to platform
    . uimage-signed-pad.bin will be generated. It is the uImage
      with signature

Image Layout
------------------------------------
U-Boot
    +-------------------+      DDR_START
    |                   |
    |    U-Boot Image   |
    |                   |
    +-------------------+      DDR_START + UBOOT_SIZE
    |    PADDING        |
    +-------------------+      align to 0x1000
    |    CSF Data       | \
    +-------------------+  +-- CSF + Pad,  Size : 0x2000
    |    PADDING        | /
    +-------------------+

uImage

    +-------------------+      DDR_START
    |                   |
    |     uImage        |
    |                   |
    +-------------------+      DDR_START + UIMAGE_SIZE
    |     PADDING       |
    +-------------------+      align to 0x1000
    |     IVT           | ---- Size : 0x20
    +-------------------+
    |     CSF Data      | \
    +-------------------+  +-- CSF + Pad,  Size : 0x2000
    |     PADDING       | /
    +-------------------+

DDR Location Parameters
------------------------------------
The DDR location parameter provided to "mk_secure_uboot" script is the
"TEXT_BASE" defined in board/freescale/<plat_name>/config.mk

	MX6Q/DL ARM2 Socket Board		MX6SL ARM2 Socket Board
	-------------------------		-------------------------
	0x27800000				0x87800000

The DDR location parameter provided to "mk_secure_uimage" script is the
"CONFIG_LOADADDR" defined in include/configs/<plat_name>.h (default). And
can be changed in u-boot command line by "setenv loadaddr=..." with valid
physical address. The following are the default values

	MX6Q/DL ARM2 Socket Board		MX6SL ARM2 Socket Board
	-------------------------		-------------------------
	0x10800000				0x80800000

Please refer to "MX6 Linux High Assurance Boot (HAB) User Guide" for
detailed test steps.