#! /bin/bash
if [ $# != 1 ]
then
	printf "	Command Syntax:\n"
	printf "	    mk_secure_bootimg <DDR_ADDR>\n"
	printf "	        DDR_ADDR : ddr address where boot.img is copied to RAM by U-Boot\n"
	printf "	Please try again\n"
	exit
fi

let ddr_addr=$1

if [ ! -f boot.img ]
then
	printf "File \"boot.img\" does not exist. Copy it from android directory and try again\n"
	exit 1
fi
printf "Make Sure Your \"boot.img\" is up to date...\n"

# DDR_ADDR should be as $(od --skip-bytes=12 --read-bytes=4  --format=x4 boot.img |head -1 | awk '{print $2}') and
# minus 0x800

# Calculate the size
let bootimg_size=$(ls -lct boot.img | awk '{print $5}')
let pad_len=$((bootimg_size - bootimg_size % 0x1000 + 0x1000)) # align to 0x1000
let auth_len=$((pad_len + 0x20)) # +0x20 "IVT"
let sig_len=$((auth_len + 0x2000))
let self_ptr=$((${ddr_addr}+ pad_len))
let csf_ptr=$((${ddr_addr} + auth_len))
let jump_addr=$((${ddr_addr} + 0x1000))

# change value to hex string
pad_len=`printf "0x%X" ${pad_len}`
auth_len=`printf "0x%X" ${auth_len}`
sig_len=`printf "0x%X" ${sig_len}`
ddr_addr=`printf "0x%X" ${ddr_addr}`
self_ptr=`printf "0x%X" ${self_ptr}`
csf_ptr=`printf "0x%X" ${csf_ptr}`
jump_addr=`printf "0x%X" ${jump_addr}`

echo "ddr_addr $ddr_addr"
echo "self_addr $self_addr"

# Create habBImagegen
sed -e s/%pad_len%/${pad_len}/g -e s/%sig_len%/${sig_len}/g ../templates/habbimagegen_template > habBImageGen
chmod +x habBImageGen

# Create BImage.csf
sed -e s/%ddr_addr%/${ddr_addr}/g -e s/%auth_len%/${auth_len}/g ../templates/bimagecsf_template > bootimg.csf

# Create genIVT
sed -e s/%jump_addr%/${jump_addr}/g -e s/%self_ptr%/${self_ptr}/g -e s/%csf_ptr%/${csf_ptr}/g ../templates/genivt_template > genIVT
chmod +x genIVT

# Generate secure boot
./habBImageGen

# Remove temperory files
rm -f genIVT habBImageGen bootimg.csf boot-pad.img ivt.bin boot-pad-ivt.img bootimg_csf.img boot-signed.img

# OK
printf "boot.img with Signature \"boot-signed-pad.img\" is ready to use\n"