FSL-UT-USB-031-Reboot-Test
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

[cols=">s,6a",frame="topbot",options="header"]
|====================================================================
|Name | Description

| Summary |
Reboot Test With U-disk Connected

| Automated |
YES

| Kernel Config Option |

| Software Dependency |
N/A

| Non-default Hardware Configuration |
N/A

| Test Procedure |
1. Put Below Commands at init script (at the end of /etc/rc.d/rcS, etc)
mount -t nfs -o nolock 10.192.244.61:/rootfs/wb /mnt/nfs
cd /mnt/nfs/vte_mx63_d/
source manual_test

/root/test_reboot.sh

NOTICE: 10.192.244.61:/rootfs/wb is the testing team VTE rootfs

2. Put the below test_reboot.sh at /root/

get_scsi.sh 4
if [ $? -eq 0 ]
then
echo "aa" >> /root/reboot_count.txt
echo "the time of reboot:"
cat /root/reboot_count.txt | wc -l
reboot
else
echo "the udisk can't be recognized"
fi

NOTICE: get_scsi.sh is the test application at VTE, it will judge
if the u-disk is existed or not.

3. Plug u-disk at USB port (Do another test with HUB connected)

4. Power up the board

| Expected Result |
The continueous reboot test can run more than 1000 iterations.

|====================================================================

<<<