FSL-UT-USB-042-USB-Peripheral-Mode-Class-Test
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

[cols=">s,6a",frame="topbot",options="header"]
|====================================================================
|Name | Description

| Summary |
Test kinds of class at peripheral mode

| Automated |
No

| Kernel Config Option |

| Software Dependency |
N/A

| Non-default Hardware Configuration |
N/A

| Test Procedure |
Since the mass storage has been tested during the role switch
test, so it only tests g_ether and g_serial

1: Test g_serial
1.1 modprobe g_serial
connect usb cable between board and pc, and you will see below message
"g_serial gadget: high-speed config #2: CDC ACM config"

1.2 Test data transfer from device to host
run "cat /dev/ttyACM0" at host side
run "echo "Happy New Year" > /dev/ttyGS0" at device side
You should see "Happy New Year" at console of host side

1.3 Test data transfer from host to device
run "cat /dev/ttyACM0" at device side
run "echo "Happy New Year" > /dev/ttyGS0" at host side
You should see "Happy New Year" at console of device side

2: Test g_ether
2.1 modprobe g_ether qmult=10
connect usb cable between board and pc, and you will see below message
"g_ether gadget: high-speed config #1: CDC Ethernet (ECM)"

2.2
At device side:
ifconfig usb0 10.0.0.2 up
At host side:
sudo ifconfig usb0 10.0.0.1 up

At device side:
ping 10.0.0.1, for ubuntu host, the ip for usb0 will lost
after several seconds, re ifconfig usb0 at host side

After ping can run more than 10 seconds, stop it

2.3 Using iperf to do ether test

At host side:
iperf -s -i 5 &
At device side:
iperf -t 1000000 -c  10.0.0.1 -d -i 5 &

2.4
The connect should be there during the overnight test
The speed is about 120Mbps.

| Expected Result |
There should be no error during the transfer

|====================================================================

<<<