FSL-UT-USB-001-HOST-Mass-Storage
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

[cols=">s,6a",frame="topbot",options="header"]
|====================================================================
|Name | Description

| Summary |
USB HOST Mass-Storage Class test

| Automated |
No

| Kernel Config Option |

| Software Dependency |
N/A

| Non-default Hardware Configuration |
N/A

| Test Procedure |
1. modprobe ehci-hcd if it's built as module. No need for MX5.

2. mkdir /mnt/udisk

3. Plug in a U-disk

4. cat /proc/partitions, e.g. major minor #blocks name 31 0 256 mtdblock0
 8 16 127744 sdb find partitions with a major that is 8, this example ,the sdb
 is U-disk partition.

5. mount -t vfat /dev/sdb /mnt/udisk

If this function is not used, unload the following drivers

umount /mnt/udisk

rmmod ehci-hcd

Note1: this test should be appled to all the ports exist on the board, for
example, OTG port, H1 port, H2 port, etc; and if there is internal hub
attached to some Host ports, for example, a internal hub is attached to Host1
, this test should be applied to the all the ports on the hub.

Note2: this test should be done for at least 10 times on every port

| Expected Result |
Pass

|====================================================================

<<<