FSL-UT-USB-003-HOST-PTP
~~~~~~~~~~~~~~~~~~~~~~~~

[cols=">s,6a",frame="topbot",options="header"]
|====================================================================
|Name | Description

| Summary |
USB HOST PTP test

| Automated |
No

| Kernel Config Option |

| Software Dependency |
N/A

| Non-default Hardware Configuration |
N/A

| Test Procedure |
How to build?

enter ptp directory. Make the PTP driver module.

make CROSS_COMPILE=${CROSS_COMPILE}

Output: usbstillimage.ko

ct ptp/test

make CROSS_COMPILE=${CROSS_COMPILE}

Ouput: ptp_test

Material: One Digital Camera (DC). Set the DC's USB mode to PTP mode.

Step:

1. modprobe ehci-hcd

2. insmod usbstillimage.ko

3. Power on DC, and connect it to the board with USB cable.

4. Download the ptp_test to the board.

chmod 777 ptp_test

/./ptp_test

If this function is not used, unload the following drivers

rmmod usbstillimage

rmmod ehci-hcd

Display: Please input command:

0: Exit

1: Display device information

2: Display storage information

3: Display file information

4: Get file

5: Get file thumbnail

6: Send a file

7: Set file protection

8: Delete file

9: Format storage

Input 1 and press Enter. It will display the device list and display the
detailed device information such as the manufacturer/model/serial number/
operations supported.

Press 2 and press Enter. It will display the detailed information of all
the storage media in the device.

Press 3 and press Enter. It will display the detailed information of all
the files (objects) in the device. The file ID for each file may be seen.
This file ID can be used in the followed file test.

Press 4 and press Enter. You will be asked to input the ID of the file to
get. Just input the hex value (no 0xprefix needed), press Enter. It will
start to get the file/object from the device, and save it to test.jpg in the
current directory on the platform. For robust test, unplug the device during
the file reading process. It will show some error message, but will not crash
. Notice that you cannot get a directory, such as MISC.

Press 5 and press Enter. You will be asked to input the ID of the file to
get the thumbnail. Just input the hex value (no 0x prefix needed), press
Enter. It will start to get the file/object thumbnail from the device, and
save it to thumb.jpg in the current directory on the platform. For robust test
, unplug the device during the file reading process. It will show some error
message but will not crash.

Press 6 and press Enter. You will be asked to input the name of the source
file to be sent from the platform to the device. Just enter the file's full
path and name and press Enter.

Then you will be asked to input the directory handle where the file is to be
put. The folder is the object with the object Association Type 1. Choose a
folder, for example "CIM" input its object handle, and press Enter. It
will start to send the file.

To keep the best compatibility, the file will be forced into the picture
format. This means that the device will treat it as a picture file and
arrange another sequence file name for it, not the source file name. After it
finishes sending the file, press 3 to show all the files, and see that a
new file has been added.
If the device is unplugged during the write process, the driver will not crash
, but sometimes the storage information on the target device will be damaged.
This is because of a design limitation of the target device. Under Windows XP/
2000 a USB device may not be unplugged when it is writing. Therefore, it is
recommended that the device not be unplugged during the write process.

Press 7 and press Enter. You will be asked to input the ID of the file to
set/clear file protection. Just input the hex value (no 0x refix needed)
and press Enter. You will be asked to input the clear or set command.

Press 1 and press Enter to set file protection (or press 0 and press
Enter to clear file protection).

Press 8 and press Enter. You will be asked to input the ID of the file to
delete. Just input the hex value (no 0x prefix needed) and press Enter. It
will try to delete the file. If the file is protected, it will show the
delete fail information.

Press 9 and press Enter. You will be asked to input the ID of the storage
to format. Just input the hex value (no 0x prefix needed) and press Enter.
It will try to format the target storage media.

To quit the test, input 0 and press Enter.

Notes: Some DCs only support read operation and don't support write operation.
On this type of DC steps 6 - 9 can't be executed, and the DC won't be able
to send a file, set file protection, delete a file or format storage.

| Expected Result |
Pass

|====================================================================

<<<