FSL-UT-USB-005-Gadget-Ethernet
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

[cols=">s,6a",frame="topbot",options="header"]
|====================================================================
|Name | Description

| Summary |
USB Gadget Ethernet test

| Automated |
No

| Kernel Config Option |

| Software Dependency |
N/A

| Non-default Hardware Configuration |
N/A

| Test Procedure |
1. insmod arcotg_udc

2. insmod g_ether

3. ifconfig usb0

4. ifconfig usb0 192.168.0.2 up When first using the USB Ethernet, and the PC
OS is Windows XP, a driver must be installed. Use the BSP file: linux\
Documentation\usb\linux.inf to install the driver.


5. On the PC (if running Windows), find a device named Linux USB Ethernet/
RNDIS Gadget

6. Configure it with a fixed IP.

7. Press the right button on the mouse, and click on TCP/IP Properties

8. Use the following IP address and settings:

	192.168.0.1

	255.255.255.0

	192.168.0.1

9.  Save these settings.

10.  From the PC, ping 192.168.0.2.

If this function is not used

ifconfig usb0 down

If this function is not used, unload the following drivers

rmmod g_ether

rmmod arcotg_udc

Note: Please run command "modprobe fsl_otg_arc" before step1 on MX25.

| Expected Result |
Basic network functions(such as Ping...) can work ok.

|====================================================================

<<<