FSL-UT-USB-006-Gadget-serial
~~~~~~~~~~~~~~~~~~~~~~~~~~

[cols=">s,6a",frame="topbot",options="header"]
|====================================================================
|Name | Description

| Summary |
USB serial gadget test

| Automated |
No

| Kernel Config Option |

| Software Dependency |
N/A

| Non-default Hardware Configuration |
N/A

| Test Procedure |
Testing the serial gadget requires windows ACM driver to be installed. This
requires gserial.inf and usbser.sys. gserial.inf can be obtained from
Documentation/usb/gadget_serial.txt. usbser.sys can be obtained using:

Expand "C:\WINDOWS\Driver Cache\i386\driver.cab" -F:usbser.sys . CAUTION: Don'
t drop the last word "." in the instructions above

Copy gserial.inf and usbser.sys to a single directory.

1. modprobe arcotg_udc

2. mknod /dev/ttyGS0 c 253 0

3. modprobe g_serial use_acm=1

	gs_bind: Gadget Serial v2.2 bound

	arcotg_udc: gadget arc_udc bound to driver g_serial

	gs_module_init: Gadget Serial v22 loaded

4. Connect the board to the PC with a USB cable.

	gs_disconnect: Gadget Serial disconnected

	gs_disconnect: Gadget Serial disconnected

	gs_set_config: Gadget Serial configured, high speed CDC-ACM config

5. Windows will recognize the serial gadget. Choose to install a driver from
a specific location and select gserial.inf. This will install usbser.sys as
the ACM driver in windows.

6. On a Windows host configure a new HyperTerminal? session to use the COM
port assigned to Gadget Serial. The "Port Settings" will be set automatically
when HyperTerminal? connects to the gadget serial device, so you can leave
them set to the default values--these settings mostly do not matter.

7. echo "hi" > /dev/ttyGS0

	String "hi" should be displayed in Gadget Serial terminal

8. cat /dev/ttyGS0

Anything you type on the Gadget Serial terminal should appear in serial port
terminal window. For further details refer to linux documentation for serial
gadget in Documentation/usb/gadget_serial.txt.

Note: Please run command "modprobe fsl_otg_arc" before step1 on MX25.

| Expected Result |
Pass

|====================================================================

<<<