FSL-UT-USB-010-UVC-TEST
~~~~~~~~~~~~~~~~~~~~~~~~

[cols=">s,6a",frame="topbot",options="header"]
|====================================================================
|Name | Description

| Summary |
USB UVC test(USB webcam support)

| Automated |
No

| Kernel Config Option |
CONFIG_USB_VIDEO_CLASS

| Software Dependency |
Ubuntu 9.04 or later

| Non-default Hardware Configuration |
N/A

| Test Procedure |
In order to test the USB UVC(USB Video Class) that is supported in Linux
kernel 2.6.24 and ongoing, please follow these procedures.

Required HW:

1. A USB camera that is supported in the UVC class. A list ofthese cameras can be
found at this URL: http://linux-uvc.berlios.de/

2. The test system should have a display of some type(DVI, VGA, or LCD).

Required SW:

1. The Linux kernel must have CONFIG_USB_VIDEO_CLASS and CONFIG_USB_EHCI_HCD selected.

2. The rootfs should a Ubuntu 9.04 or later.

Test Procedure:

1. Boot up the Linux kernel with the Ubuntu file system.

2. Use the Apps search tool to download and install a webcam application
(such as xawtv or cheese).

3. Plug in the webcam into a USB host port on the development system.

4. Launch the webcam application and use the viewfinder. The application
should find the USB webcam automatically

| Expected Result |
Pass

|====================================================================

<<<