FSL-UT-USB-012-HOST-Remote-Wakeup
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

[cols=">s,6a",frame="topbot",options="header"]
|====================================================================
|Name | Description

| Summary |
USB Host: Remote Wakeup system

| Automated |
No

| Kernel Config Option |

| Software Dependency |
N/A

| Non-default Hardware Configuration |
N/A

| Test Procedure |

Take usb otg host as an example:

Plug a mouse to the otg port (take otg as an example)

cat /sys/device/platform/fsl-usb2-otg/power/wakeup

disabled

cat /sys/bus/usb/device/1-1/power/wakeup

disabled

echo mem > /sys/power/state

	......

press the button on the mouse, system can not be waked up

echo enabled > /sys/devices/platform/fsl-usb2-otg/power/wakeup

echo enabled > /sys/devices/platform/fsl-ehci.0/power/wakeup

echo mem > /sys/power/state

press the button on the mouse, system can not be waked up if 2.6.35 kernel is
used, and system can be waked up with 2.6.31

below is for 2.6.35

	......

echo enabled > /sys/device/platform/fsl-usb2-otg/power/wakeup

echo enabled > /sys/devices/platform/fsl-ehci.0/power/wakeup

echo enabled > /sys/bus/usb/device/1-1/power/wakeup

echo mem > /sys/power/state

press the button on the mouse, system can be waked up

Take usb host1 as an example

cat /sys/device/platform/fsl-ehci.1/power/wakeup

disabled

echo mem > /sys/power/state

	......

insert a udisk, system can not be waked up.

echo enabled > /sys/device/platform/fsl-ehci.1/power/wakeup

cat /sys/device/platform/fsl-usb2-udc/power/wakeup

enabled

echo mem > /sys/power/state

	......

insert a udisk, system can be waked up.


echo mem > /sys/power/state

	......

remove the udisk, system can be waked up

same tests need to be done on any other host port, for example, the
internal hub attached to the Host1 port on mx53, mx6q, so all the exported
port on the internal hub need to test.

| Expected Result |
Pass

|====================================================================

<<<