FSL-UT-V4L2-003
~~~~~~~~~~~~~~~

[cols=">s,6a",frame="topbot",options="header"]
|====================================================================
|Name | Description

| Summary |
camera preview

| Automated |
NO

| Kernel Config Option |
N/A

| Software Dependency |
N/A

| Non-default Hardware Configuration |
A camera and display are required.

| Test Procedure |

Check that /dev/video0 exists. If it does not exist, load the camera driver with the command:

 modprobe mxc_v4l2_capture

modprobe CAMERA_MODULE (CAMERA_MODULE should be replaced by the camera module on the related platform, e.g. ov3640_camera should be used here on MX51)

Check again for /dev/video0. If it is not there, the camera driver has not loaded successfully and the test has failed.

Type the following command.

 mxc_v4l2_overlay.out -iw 640 -ih 480 -it 0 -il 0 -ow 160 -oh 160 -ot 20 -ol 20 -r 0 -t 50 -do 0 -fg -fr 30

Direct preview the camera to the foreground, and set the frame rate to 30 fps, the window of interest is 640 X 480 with a starting offset of (0,0), the preview size is 160 X 160 with a starting offset of (20,20). Use mxc_v4l2_overlay.out -help to see usage.

| Expected Result |
The image from the camera is displayed on the screen. Colors and image should be correct.

|====================================================================

<<<