FSL-UT-V4L2-008
~~~~~~~~~~~~~~~

[cols=">s,6a",frame="topbot",options="header"]
|====================================================================
|Name | Description

| Summary |
MIPI CSI preview

| Automated |
NO

| Kernel Config Option |
N/A

| Software Dependency |
N/A

| Non-default Hardware Configuration |
ov5640 sensor and MIPI extention board are requried display screen also is needed

| Test Procedure |
Check that /dev/video1 exists. If it does not exist, load the camera driver with the command:

modprobe mxc_v4l2_capture

modprobe CAMERA_MODULE (CAMERA_MODULE should be replaced by the camera module on the related platform, e.g. ov5640_camera_mipi should be used here on MX6Q)

Check again for /dev/video1. If it is not there, the camera driver has not loaded successfully and the test has failed.

Type commands to direct preview the camera to the foreground/background, and set the frame rate to 30 fps, the preview size is 640 X 480 with a starting offset of (0,0). Use mxc_v4l2_overlay.out -help to see usage.

Test foreground display:

Test 1. mxc_v4l2_overlay.out -iw 640 -ih 480 -ow 640 -oh 480 -m 0 -di /dev/video1 -fg

Test 2. mxc_v4l2_overlay.out -iw 320 -ih 240 -ow 640 -oh 480 -m 1 -di /dev/video1 -fg

Test 3. mxc_v4l2_overlay.out -iw 720 -ih 480 -ow 640 -oh 480 -m 2 -di /dev/video1 -fg

Test 4. mxc_v4l2_overlay.out -iw 720 -ih 576 -ow 640 -oh 480 -m 3 -di /dev/video1 -fg

Test 5. mxc_v4l2_overlay.out -iw 1280 -ih 720 -ow 640 -oh 480 -m 4 -di /dev/video1 -fg

Test 6. mxc_v4l2_overlay.out -iw 1920 -ih 1080 -ow 640 -oh 480 -m 5 -di /dev/video1 -fg

Test 7. mxc_v4l2_overlay.out -iw 2592 -ih 1944 -ow 640 -oh 480 -m 6 -fr 15 -di /dev/video1 -fg

Test background display:

Test 8. mxc_v4l2_overlay.out -iw 640 -ih 480 -ow 640 -oh 480 -m 0 -di /dev/video1 -bg

Test 9. mxc_v4l2_overlay.out -iw 320 -ih 240 -ow 640 -oh 480 -m 1 -di /dev/video1 -bg

Test 10. mxc_v4l2_overlay.out -iw 720 -ih 480 -ow 640 -oh 480 -m 2 -di /dev/video1 -bg

Test 11. mxc_v4l2_overlay.out -iw 720 -ih 576 -ow 640 -oh 480 -m 3 -di /dev/video1 -bg

Test 12. mxc_v4l2_overlay.out -iw 1280 -ih 720 -ow 640 -oh 480 -m 4 -di /dev/video1 -bg

Test 13. mxc_v4l2_overlay.out -iw 1920 -ih 1080 -ow 640 -oh 480 -m 5 -di /dev/video1 -bg

Test 14. mxc_v4l2_overlay.out -iw 2592 -ih 1944 -ow 640 -oh 480 -m 6 -fr 15 -di /dev/video1 -bg

| Expected Result |
The image from the camera is displayed on the screen. Colors and image should be correct.

|====================================================================

<<<