FSL-UT-V4L2-009
~~~~~~~~~~~~~~~

[cols=">s,6a",frame="topbot",options="header"]
|====================================================================
|Name | Description

| Summary |
MIPI CSI Capture

| Automated |
NO

| Kernel Config Option |
N/A

| Software Dependency |
N/A

| Non-default Hardware Configuration |
ov5640 sensor and MIPI extention board are requried

| Test Procedure |
Check that /dev/video1 exists. If it does not exist, load the camera driver with the command: modprobe mxc_v4l2_capture

modprobe CAMERA_MODULE (CAMERA_MODULE should be replaced by the camera module on the related platform, e.g. ov5640_camera_mipi should be used here on MX6Q).

Check again for /dev/video1. If it is not there, the camera driver has not loaded successfully and the test has failed.

Type the following command lines in a writable directory. The 50 frames of video from the camera will be captured in the file "test.yuv" for each resolution. The format will be YUV420.

Test CSI->SMFC->MEM:

Test 1. mxc_v4l2_capture.out -iw 640 -ih 480 -ow 640 -oh 480 -m 0 -i 1 -r 0 -c 50 -fr 30 -d /dev/video1 test.yuv

Test 2. mxc_v4l2_capture.out -iw 320 -ih 240 -ow 320 -oh 240 -m 1 -i 1 -r 0 -c 50 -fr 30 -d /dev/video1 test.yuv

Test 3. mxc_v4l2_capture.out -iw 720 -ih 480 -ow 720 -oh 480 -m 2 -i 1 -r 0 -c 50 -fr 30 -d /dev/video1 test.yuv

Test 4. mxc_v4l2_capture.out -iw 720 -ih 576 -ow 720 -oh 576 -m 3 -i 1 -r 0 -c 50 -fr 30 -d /dev/video1 test.yuv

Test 5. mxc_v4l2_capture.out -iw 1280 -ih 720 -ow 1280 -oh 720 -m 4 -i 1 -r 0 -c 50 -fr 30 -d /dev/video1 test.yuv

Test 6. mxc_v4l2_capture.out -iw 1920 -ih 1080 -ow 1920 -oh 1080 -m 5 -i 1 -r 0 -c 50 -fr 30 -d /dev/video1 test.yuv

Test 7. mxc_v4l2_capture.out -iw 2592 -ih 1944 -ow 2592 -oh 1944 -m 6 -i 1 -r 0 -c 50 -fr 15 -d /dev/video1 test.yuv

Test CSI->PRP->MEM:

Test 8. mxc_v4l2_capture.out -iw 640 -ih 480 -ow 640 -oh 480 -m 0 -r 0 -c 50 -fr 30 -d /dev/video1 test.yuv

Test 9. mxc_v4l2_capture.out -iw 320 -ih 240 -ow 640 -oh 480 -m 1 -r 0 -c 50 -fr 30 -d /dev/video1 test.yuv

Test 10. mxc_v4l2_capture.out -iw 720 -ih 480 -ow 640 -oh 480 -m 2 -r 0 -c 50 -fr 30 -d /dev/video1 test.yuv

Test 11. mxc_v4l2_capture.out -iw 720 -ih 576 -ow 640 -oh 480 -m 3 -r 0 -c 50 -fr 30 -d /dev/video1 test.yuv

Test 12. mxc_v4l2_capture.out -iw 1280 -ih 720 -ow 640 -oh 480 -m 4 -r 0 -c 50 -fr 30 -d /dev/video1 test.yuv

Test 13. mxc_v4l2_capture.out -iw 1920 -ih 1080 -ow 640 -oh 480 -m 5 -r 0 -c 50 -fr 30 -d /dev/video1 test.yuv

Test 14. mxc_v4l2_capture.out -iw 2592 -ih 1944 -ow 640 -oh 480 -m 6 -r 0 -c 50 -fr 15 -d /dev/video1 test.yuv

| Expected Result |
There should be no errors or warnings. The file "test.yuv" will be created.

To display the video at the resolution of 640x480, use the command line below (a different resolution may be used depending on display size), then verify captured file contents match viewfinder and that the image is clear and the colors correct.

For Test 1. mxc_v4l2_output.out -iw 640 -ih 480 -ow 640 -oh 480 -r 0 -fr 30 test.yuv

For Test 2. mxc_v4l2_output.out -iw 320 -ih 240 -ow 640 -oh 480 -r 0 -fr 30 test.yuv

For Test 3. mxc_v4l2_output.out -iw 720 -ih 480 -ow 640 -oh 480 -r 0 -fr 30 test.yuv

For Test 4. mxc_v4l2_output.out -iw 720 -ih 576 -ow 640 -oh 480 -r 0 -fr 30 test.yuv

For Test 5. mxc_v4l2_output.out -iw 1280 -ih 720 -ow 640 -oh 480 -r 0 -fr 30 test.yuv

For Test 6. mxc_v4l2_output.out -iw 1920 -ih 1080 -ow 640 -oh 480 -r 0 -fr 30 test.yuv

For Test 7. mxc_v4l2_output.out -iw 2592 -ih 1944 -ow 640 -oh 480 -r 0 -fr 15 test.yuv

For Test 8-13. mxc_v4l2_output.out -iw 640 -ih 480 -ow 640 -oh 480 -r 0 -fr 30 test.yuv

For Test 14. mxc_v4l2_output.out -iw 640 -ih 480 -ow 640 -oh 480 -r 0 -fr 15 test.yuv

|====================================================================

<<<