FSL-UT-PM-007-CPUFREQ
~~~~~~~~~~~~~~~~~~~~~

[cols=">s,6a",frame="topbot",options="header"]
|====================================================================
|Name | Description

| Summary |
CPUFREQ TEST

| Automated |
No

| Kernel Config Option |
N/A

| Software Dependency |
N/A

| Non-default Hardware Configuration |
N/A

| Test Procedure |
. Make sure if CPUFREQ governor is userspace:

 cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor
 userspace

. If yes, go to step 3. otherwise, do the following:

 echo userspace > /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor

. To show current CPU frequency in KHz (e.g. 392727 KHz):

 cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_cur_freq
 392727

. To show current CPU voltage in uV (e.g. 1450000 uV):

 cat /sys/class/regulator/regulator.0/microvolts
 1450000

. To show the minimum CPU frequency (e.g. 261818 KHz) can be changed:

 cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_min_freq
 261818

. To change CPU frequency to the minimum frequency (e.g. 261818 KHz):

 echo 261818 > /sys/devices/system/cpu/cpu0/cpufreq/scaling_setspeed

.  To show current CPU frequency in KHz (e.g. 261818 KHz):

 cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_cur_freq
 261818

. To show current CPU voltage in uV (e.g. 1275000 uV):

 cat /sys/class/regulator/regulator.0/microvolts
 1275000

. To show the maximum CPU frequency (e.g. 454736 KHz) can be changed:

 cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_max_freq
 454736

. To change CPU frequency to the maximum frequency (e.g. 454736 KHz):

 echo 454736 > /sys/devices/system/cpu/cpu0/cpufreq/scaling_setspeed

. To show current CPU frequency in KHz (e.g. 454736 KHz):

 cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_cur_freq
 454736

. To show current CPU voltage in uV (e.g. 1550000 uV):

 cat /sys/class/regulator/regulator.0/microvolts
 1550000

. To show what values of CPU frequency can be changed in KHz (The first value of each row is the frequency value can be changed into):

 cat /sys/devices/system/cpu/cpu0/cpufreq/stats/time_in_state

| Expected Result |
.The CPU frequency should be changed to the value requested. The CPU voltage should be changed.

. After changing CPU frequency to the value listed by using the thirteenth command above (ex. 996 MHz), the CPU voltage should be around 1.225V by measuring VDDARM on CPU card and ground. To see the current cpu freq you can use the third command above.

. After changing CPU frequency to to the value listed by using the thirteenth command above (ex. 198MHz), the CPU voltage should be around 0.85V (1.00V for i.MX6DL-ARM2) by measuring VDDARM on CPU card and ground. To see the current cpu freq you can use the third command above.

|====================================================================

<<<