Model history
Since the updates for SiMKit 3.1 (May 2008) the code history is included in the model history. Older code history can be found below.
Bipolar Model Modella 500
Below is an overview of the relation between level and code versions. The background of the compact model identification scheme can be read here .
| Modella | SiMKit | ||
|---|---|---|---|
| level.version.implementation | code revision | release | date |
| 500.0.14 | 1.93 | 3.8 | 2012-02-02 |
| 500.0.13 | 1.91.2.1 | 3.7 | 2011-08-04 |
| 500.0.12 | 1.73.2.1 | 3.6 | 2011-01-18 |
| 500.0.11 | 1.70 | 3.5.2 | 2010-10-12 |
| 500.0.10 | 1.62 | 3.4 | 2009-12-17 |
| 500.0.9 | 1.60 | 3.2, 3.3 | 2009-06-25 |
| 500.0.8 | 1.58 | 3.1.2 | 2008-07-24 |
| 500.0.8 | 1.58 | 3.1 | 2008-05-21 |
| 500.0.7 | 1.50.2.1 | 3.0.2 | 2008-01-31 |
| 500.0.6 | 1.37 | 2.5 | 2007-04-30 |
| 500.0.5 | 1.34 | 2.4 | 2006-10-23 |
| 500.0.4 | 1.25 | 2.3 | 2006-03-16 |
| 500.0.3 | 1.19 | 2.2 | 2005-08-03 |
| 500.0.2 | 1.15 | 2.1.1 | 2005-04-11 |
| 500.0.1 | 1.1 | 2.0.1 | 2004-11-17 |
| 2011/08 | The model has been made thread-safe |
| 2011/01 | Minor code change: Situations where “pow()”, calculating x^y with y==0.5 are now avoided by using the sqrt() function. |
| 2005/04 | Self-heating has been included in the model. |
| 1990 | Introduction of Modella. |
Code history
Bipolar Model Modella 500
The table below outlines the major changes to the file called "device_tpl500i.c", which can be found in the source code.
| 2008/12 | Release of Modella, 500.0.9 |
| |
| 2008/05 | Release of Modella, 500.0.8 |
| |
| 2008/01/31 | Mextram 500.0.7. |
| Code changes | |
| |
| 2007/04/30 | Modella 500.0.6 is identified in the code as revision 1.37. All code differences with the previous version (500.0.5) can be found in this diff file. |
| Minor code changes | |
| 2006/10/23 | Modella 500.0.5 identified in the code as revision 1.34. All code differences wit the previous version (500.0.4) can be found in this diff file. |
| Implemented model changes | |
| None | |
| Minor code changes | |
| |
| 2006/03/16 | Modella 500.0.4, which is identified in the code as revision 1.25. All code differences with the previous version (500.0.3) can be found in this diff file. |
| Implemented model changes | |
| None | |
| Other code changes | |
| Code changes to improve numerical robustness | |
| 2005/08/03 | Modella 500.0.3, which is identified in the code as revision 1.19. All code differences with the previous version (500.0.2) can be found in this diff file. |
| Implemented model changes | |
| None | |
| Other code changes | |
| Implementation of internal diffusion voltage has been changed | |
| 2005/04/11 | Modella Model 500.0.2 identified in the code as revision 1.15. All code differences with the previous version (500.0.1) can be found in this diff file. |
| Implemented model changes | |
| |
| Other code changes | |
| None | |
| 1990 | Release of Modella level 500. |
Known bugs
There are no known bugs in Modella.




Follow us