Model history
Since the updates for SiMKit 3.1 (May 2008) the code history is included in the model history. Older code history can be found below.
MOS model 2002
Below is an overview of the relation between level and code versions.
The background of the compact model identification scheme can be read here.
| MOS2002 | SiMKit | ||
|---|---|---|---|
| level.version.implementation | code revision | release | date |
| 2002.2.7 | 1.85 | 3.7 | 2011-08-04 |
| 2002.2.7 | 1.81 | 3.6 | 2011-01-18 |
| 2002.2.6 | 1.76 | 3.5.2 | 2010-01-12 |
| 2002.2.5 | 1.62 | 3.4 | 2009-12-17 |
| 2002.2.4 | 1.58 | 3.3 | 2009-06-25 |
| 2002.2.3 | 1.56.2 | 3.2 | 2008-12-02 |
| 2002.2.2 | 1.54 | 3.1.2 | 2008-07-24 |
| 2002.2.2 | 1.54 | 3.1 | 2008-05-11 |
| 2002.2.1 | 1.44.2.1 | 3.0.3 | 2008-01-31 |
| 2002.2.0 | 1.29 | 2.5 | 2007-04-30 |
| 2002.1.0 | 1.21 | 2.4 | 2006-10-23 |
| 2002.0.0 | 1.6 | 2.3 | 2006-07-07 |
| 2011/01 | Release of MOS MODEL 20, 2002.2.7 |
| |
| 2010/10 | Release of MOS MODEL 20, 2002.2.6 |
| |
| 2009/12 | Release of MOS MODEL 20, 2002.2.5 |
| 2009/06 | Release of MOS MODEL 20, 2002.2.4 |
| |
| 2008/12 | Release of MOS MODEL 20, 2002.2.3 |
| |
| 2008/05 | Release of MOS MODEL 20, 2002.2.2 |
| |
| 2007/04 | Release of MOS MODEL 20, 2002.2.0 |
| |
| 2006/10 | Release of MOS MODEL 20, 2002.1.0 |
| Avalanche current of the drift region has been included in the model. Please note that some parameters have a new name, and some parameters have been added. Details can be found in the Modelbook. | |
| 2006/03 | Release of MOS MODEL 20, 2002.0.0 |
| Release of MOS Model 20, level 2002 is available as a test version. Release of MOS Model 20, level 2002 is available as a test version. Velocity saturation in the drift region has been included. |
MOS model 2001
Below is an overview of the relation between level and code versions.
The background of the compact model identification scheme can be read here.
| MOS2001 | SiMKit | ||
|---|---|---|---|
| level.version.implementation | code revision | release | date |
| 2001.0.9 | 1.169 | 3.3 | 2009-06-25 |
| 2001.0.8 | 1.167.2 | 3.2 | 2008-12-02 |
| 2001.0.7 | 1.165 | 3.1.2 | 2008-07-24 |
| 2001.0.7 | 1.165 | 3.1 | 2008-05-21 |
| 2001.0.6 | 1.153.2.1 | 3.0.3 | 2008-01-31 |
| 2001.0.5 | 1.138 | 2.5 | 2007-04-30 |
| 2001.0.4 | 1.130 | 2.4 | 2006-10-23 |
| 2001.0.3 | 1.117 | 2.3 | 2006-03-16 |
| 2001.0.2 | 1.107 | 2.2 | 2005-08-03 |
| 2001.0.1 | 1.104 | 2.1.1 | 2005-04-11 |
| 2001.0.0 | 1.78 | 2.0.1 | 2004-11-17 |
The table below outlines the major changes to the file called "device_m2001i.c".
| 2009/12 | MOS MODEL 20, 2001 will be no part of SiMKit 3.4, nor of any future SiMKits |
| 2009/06 | Release of MOS MODEL 20, 2001.0.9 |
| |
| 2008/12 | Release of MOS MODEL 20, 2001.0.8 |
| |
| 2008/05 | Release of MOS MODEL 20, 2001.0.7 |
| The output units of the parameters KOD and KODR have been corrected to V^1/2 | |
| 2007/04 | Release of MOS MODEL 20, 2001.0.5 |
| The clipping of the effective width of the transistor was not handled correctly, which ended up in an error when the effective width became less than, or equal to, 0. This is solved now by clipping the width in the correct way. | |
| 2005/04 | Release of MOS MODEL 20, 2001.0.1 |
| Self-heating has been included in the model. | |
| 2004/10 | Release of MOS MODEL 20, 2001.0.0 |
| This update includes some practical changes, like the pinch-off voltage Voxp0, the clip-low value of m and of lD, and the implementation of the noise transfer function. | |
| 2004/01 | Release of MOS MODEL 20, 2001.0, test version |
| This update omits the source-drain interchange for the dc-current description. | |
| 2003/10 | Release of MOS MODEL 20, 2001.0, test version |
Code history
MOS model 2002
The table below outlines the major changes to the file called "device_m2002i.c", which can be found in the source code.
| 2008/01/31 | MOS Model 2002.2.1. |
| Code changes | |
| |
| 2007/04/30 | MOS Model 2002.2.0 is identified in the code as revision 1.29. All code differences with the previous version (1100.3.6) can be found in this diff file. |
| Implemented model changes | |
| |
| Minor code changes | |
| 2006/10/23 | MOS Model 2002.1.0 identified in the code as revision 1.21. All code differences with the previous version (2002.0.0) can be found in this diff file. |
| Implemented model changes | |
| |
| Other code changes | |
| Minor code changes | |
|
MOS model 2001
| 2008/01/31 | MOS Model 2001.0.6. |
| Code changes | |
| |
| 2007/04/30 | MOS Model 2001.0.5 is identified in the code as revision 1.138. All code differences with the previous version (1100.3.6) can be found in this diff file. |
| Implemented model changes | |
| |
| Minor code changes | |
| 2006/10/23 | MOS model 2001.0.4 identified in the code as revision 1.130. All code differences with the previous version (2001.0.3) can be found in this diff file. |
| Implemented model changes | |
| |
| Minor code changes | |
| |
| 2006/03/16 | MOS Model 2001.0.3 identified in the code as revision 1.117. All code differences with the previous version (2001.0.2) can be found in this diff file. |
| Implemented model changes | |
| |
| Other code changes | |
| Minor code changes | |
| 2005/08/03 | MOS Model 2001.0.2 identified in the code as revision 1.107. All code differences with the previous version (2001.0.1) can be found in this diff file. |
| Implemented model changes | |
| |
| Other code changes | |
| Minor code changes | |
| 2005/04/11 | MOS Model 2001.0.1 identified in the code as revision 1.104. All code differences with the previous version (2001.0.0) can be found in this diff file. |
| Implemented model changes | |
| |
| Other code changes | |
| Convergence problems solved by correcting the implementation of derivatives of Ddibl . Wrong clipping values corrected for LAMD | |
| 2004/11/17 | Introduction of MOS MODEL 20, level 2001. |
| This update includes some practical changes, like the pinch-off voltage Voxp0, the clip-low value of m and of lD, and the implementation of the noise transfer function. | |
| 2004/01 | Update of MOS model 20, level 2001, test version |
| This update omits the source-drain interchange for the dc-current description. | |
| 2003/10 | Release of MOS Model 20, level 2001, test version |
Known bugs
There are no known bugs in MOS Model 20, level 2001.




Follow us