NXP Semiconductors logo
Select site:
English
MOS Model 31


Introduction to MOS Model 31

MOS Model 31 is a physics based transistor model to be used in circuit simulation and IC-design of analogue high-voltage applications. The model describes the electrical behaviour of a junction-isolated accumulation/depletion-type MOSFET. The model is used as the drain extension of high-voltage MOS devices, like the Lateral Double-diffused MOS (LDMOS), the Vertical Double-diffused MOS (VDMOS), and the Extended MOS transistors.


Read more about MOS Model 31.

Model definition of MOS Model 31

The model definition of MOS Model 31 is available as PDF files:



The history of MOS Model 31 can be found here.

Source Code & Library

The source code of MOS Model 30 and the source code of MOS Model 31 are available here. The file containing the MOS Model 31 code is called "device_m3100.c", while the file "device_m30.c" contains the MOS Model 30 code. If you use the included solver, please make sure that you compile on a system that supports Fortran 77.


The history of the source code can be found here.


The models are included in a dynamically loaded library called SiMKit.


SiMKit is related to the following circuit simulators used within NXP:


  • Pstar, the circuit simulator from NXP
  • Spectre, the circuit simulator from Cadence
  • ADS, the circuit simulator from Agilent.

You can read how to download and install the libraries here.


The source code is protected by Copyright © 1991, 2007, NXP.

Additional documentation

There is no additional documentation on MOS Model 31 available.

Related publications

Further information on MOS Model 31 is available in the following related publications:



© 2001, 2006 IEEE. Personal use of this material is permitted. However, permission to reprint/republish this material for advertising or promotional purposes or for creating new collective works for resale or redistribution to servers or lists, or to reuse any copyrighted component of this work in other works must be obtained from the IEEE.