NXP Semiconductors logo
Select site:
English
MOS model 11


Introduction to MOS Model 11

MOS Model 11 has been developed as the successor of MOS Model 9. The development goals for MOS Model 11 have been:


  • suitable for digital, analog and RF;
  • suitable for modern and future CMOS technologies;
  • physics based;
  • number of parameters comparable to MOS Model 9;
  • simulation time comparable to MOS Model 9; and
  • simple parameter extraction.

Read more about MOS Model 11.

Model definition of MOS Model 11

The model definition of MOS Model 11, Download PDF File Level 1102 (1.89MB) Download PDF File Level 1101 (1.70MB) and Download PDF File Level 1100 (1.17MB) are available in PDF format, as well as a definition of the Download PDF File hyp functions (113KB) used in this model.


The history of the model can be found here.


MOS Model 11, Level 1101, is an updated version of Level 1100. It uses the same basic equations as Level 1100, but uses different geometry scaling rules. It includes two types of geometrical scaling rules: physical rules and binning rules. Moreover, the temperature scaling has been implemented on the "miniset" level instead of the "maxiset" level as is the case for Level 1100.


MOS Model 11, Level 1102, is an updated version of Level 1101. It uses the same parameter set and parameter scaling relations as Level 1101, but uses slightly different model equations. The surface potential is calculated iteratively using a second-order Newton-Raphson procedure, resulting in a more accurate description of surface potential. Owing to the increased accuracy, some of the basic equations used in Level 1101 can be simplified, and as a result Level 1102 is computationally as fast as Level 1101. In addition, a more physical and simpler velocity saturation expression is used, and as a consequence the saturation voltage expression has changed slightly as well. This all results in a more accurate description of transconductance in saturation. Finally, more accurate physics-based equations have been implemented in Level 1102 for thermal noise, induced gate noise and their correlation.


The description of the source-bulk and drain-bulk junction diode is not included in MOS Model 11. The behaviour of these junction diodes is modelled by the Juncap model. This model has to be added between the source and bulk node and between the drain and bulk node.

Source Code & Library

The source code of MOS Model 11 is available here. The files containing the "Level 1100" code, the "Level 1101" code and the "Level 1102" code are "device_m1100.c", "device_m1101.c" and "device_m1102.c" respectively. If you use the included solver, please make sure that you compile on a system that supports Fortran 77.


The history of the source code can be found here.


The models are included in a dynamic loaded library called SiMKit.


SiMKit is related to the following circuit simulators used within NXP:


  • Pstar, the circuit simulator from NXP
  • Spectre, the circuit simulator from Cadence
  • ADS, the circuit simulator from Agilent.

You can read how to download and install the libraries here.


The source code is protected by Copyright © 1991, 2007, NXP.

Additional documentation

Further information on MOS Model 11 is available in the following additional reports:


Related Publications

Further information on MOS Model 11 is available in the following related publications:



© 1997, 2007 IEEE. Personal use of this material is permitted. However, permission to reprint/republish this material for advertising or promotional purposes or for creating new collective works for resale or redistribution to servers or lists, or to reuse any copyrighted component of this work in other works must be obtained from the IEEE.