NXP Semiconductors logo
Select site:
English
MOS model 9


Introduction to MOS Model 9

MOS Model 9 is a physics based analytical model for electrical circuit simulation and design for analogue applications. It provides an excellent description of the electrical characteristics in all relevant regions of transistor operation such as the sub-threshold current, the substrate current and the output conductance.


MOS Model 9 describes transistor behaviour over a wide range of channel lengths and widths using just one parameter set. Thereby making it easy and flexible to use across a broad spectrum of applications, while maintaining consistently high accuracy. The full documentation and source code of MOS Model 9 is freely available from this website.


Initially developed for use with Pstar, the NXP analogue circuit simulator, MOS Model 9 is suitable for use both in circuit design and process technology, as well as in CAD tool development.


Read more about MOS Model 9.

Model definition of MOS Model 9

The model definition of MOS Model 9, Download PDF File Level 902 (782Kb) and Download PDF File Level 903 (1.19MB) are available in PDF format, as well as a definition of the Download PDF File hyp functions (113KB) used in this model.


The history of the model can be found here.


The description of the source-bulk and drain-bulk junction diode is not included in MOS Model 9. The behaviour of these junction diodes is modelled by the Juncap (152kB) model. This model has to be added between the source and bulk node and between the drain and bulk node

Source Code & Library

The source code of MOS Model 9 is available here.


The files called "device_m902.c" and "device_m903.c" contain the majority of the MOS Model 9 code. If you use the included solver, please make sure that you compile on a system that supports Fortran 77.


The history of the source code can be found here.


The models are included in a dynamically loaded library called SiMKit.


SiMKit is related to the following circuit simulators used within NXP:


  • Pstar, the circuit simulator from NXP
  • Spectre, the circuit simulator from Cadence

MOS model 9 is not available for the ADS simulator.


You can read how to download and install the libraries here.


The source code is protected by Copyright © 1991, 2007, NXP.

Additional documentation

Further information on MOS Model 9 is available in the following additional documentation:


Related publications

Further information on MOS Model 9 is available in the following related publications:


  • Download PDF File "Impact of Process Scaling on 1/f Noise in Advanced CMOS Technologies", M.J. Knitel, P.H. Woerlee, A.J. Scholten, and A.T.A. Zegers - van Duijnhoven, IEDM Techn. Digest (San Francisco), pp. 463-466, 2000 (250kB).
  • "Effect of dogbone geometry on source/drain resistance in narrow-width MOSFETs", A.J. Scholten and D.B.M. Klaassen, Solid-State Electronics 43, pp.1989-1996 (1999).
  • Download PDF File "Anomalous geometry dependence of source/drain resistance in narrow-width MOSFETs", A.J. Scholten and D.B.M. Klaassen, Proceedings of the IC-MTS'98, pp. 77-82, 1998 (427kB).
  • Download PDF File "Statistical characterization of 0.18 micron low-power CMOS process using efficient parameter extraction", K.G. McCarthy, E.V. Saavedra Diaz, D.B.M. Klaassen and A. Mathewson, Proceedings of the IC-MTS'98 (343kB).
  • Download PDF File "RF noise modelling of 0.25 micron CMOS and low-power LNA's", R.R.J. Vanoppen, L.M.F. de Maaijer, D.B.M. Klaassen and L.F. Tiemeijer, IEDM Techn. Digest (Washington, DC), pp. 317-320, 1997 (294kB).
  • "Efficient parameter extraction and statistical analysis for a 0.25 micron low-power CMOS process", E.V. Saavedra Diaz, K.G. McCarthy, D.B.M. Klaassen and A. Mathewson, Proceedings of the 27th European Solid-State Device Research Conference (ESSDERC'97), pp. 656-659, Edition Frontieres, 1997.
  • Download PDF File "Circuit Sensitivity Analysis in Terms of Process Parameters", M.J. van Dort and D.B.M. Klaassen, IEDM Techn. Digest (Washington, DC), pp. 941-944, 1995 (278kB).
  • "Prediction of compact MOS model parameters for low-power application", R.M.D.A. Velghe and D.B.M. Klaassen, Proceedings of the 25th European Solid-State Device Research Conference (ESSDERC'95), pp. 565-568, Edition Frontieres, 1995.
  • "Sensitivity Analysis of an Industrial CMOS Process using RSM Techniques", M.J. van Dort and D.B.M. Klaassen, Proc. SISDEP, pp. 432-435, 1995.
  • Download PDF File "The high-frequency analogue performance of MOSFETs", R.R.J. Vanoppen, J.A.M. Geelen and D.B.M. Klaassen, IEDM Techn. Digest (San Francisco, CA), pp. 173-176, 1994 (252kB).
  • "Compact Modelling for Analogue Circuit Simulation", R.M.D.A. Velghe, D.B.M. Klaassen and F.M. Klaassen, Proceedings of the 24th European Solid-State Device Research Conference (ESSDERC'94), pp. 833-836, Edition Frontieres, 1994.
  • Download PDF File "Compact Modelling for Analogue Circuit Simulation", R.M.D.A. Velghe, D.B.M. Klaassen and F.M. Klaassen, IEDM Techn. Digest (Washington, DC), pp. 485-488, 1993 (278kB).
  • "Compact Transistor Modelling for Circuit Design", by H.C. de Graaff and F.M. Klaassen, Springer, 1990.

© 1990, 2006 IEEE. Personal use of this material is permitted. However, permission to reprint/republish this material for advertising or promotional purposes or for creating new collective works for resale or redistribution to servers or lists, or to reuse any copyrighted component of this work in other works must be obtained from the IEEE.