NXP Semiconductors logo
Select site:
English
News Archive


2008/02/01 : SiMKit 3.0.3 released!

A new version of the SiMKit library is now available. The SIMKit interface has been redesigned to allow models with a flexible topology. PSP is the first model to make use of the flexibility.


Download PDF File Read more about SiMKit 3.0.3.


Download PDF File Read more about SiMKit 2.5.


2006/10/23 : SiMKit 2.4 released!

A new version of the SiMKit library is now available.


Download PDF File Read more about SiMKit 2.4.


2006/07/07 : SiMKit 2.3.2 released!

A new version of the SiMKit library is now available. The new SiMKit contains PSP level 102.0, which is the first CMC standard version of PSP. In this SiMKit version previous versions of PSP are not supported.


Download PDF File Read more about SiMKit 2.3.2.


SiMKit is related to the circuit simulators Pstar, Spectre and ADS. Downloads and information about how to install the SiMKit libraries can be found here.

2006/03/16 : SiMKit 2.3 released!

A new version of the SiMKit library is now available. The new SiMKit contains PSP level 101 which is the succesor to PSP level 100. This new version is not backwards compatible with the previous version. In this SiMKit version, only level 101 of PSP models is supported.


A new model description for the compact high-voltage MOS transistor model called MOS Model 20, level 2002 is available as a test version.


Download PDF File Read more about SiMKit.


SiMKit is related to the circuit simulators Pstar, Spectre and ADS. Downloads and information about how to install the SiMKit libraries can be found here.


Note that the updated version of the bipolar model book and the MOS model book, based on SiMKit 2.3, are now available on this website. Please also notice that the documentation of PSP101 and MM2002 are not in the model books but are available in the form of Natlab technical notes.

2005/08/03 : SiMKit 2.2 released!

A new version of the SiMKit library is now available. MOS model PSP level 100 and Juncap level 200 are improved.


Download PDF File Read more about SiMKit


SiMKit is related to the circuit simulators Pstar, Spectre and ADS. Downloads and information about how to install the SiMKit libraries can be found here.


Note that the release of the bipolar model book and the MOS model book, based on SiMKit 2.2, will be released in Q4 of this year. The update of the models is described in reports that are available on this website.

2005/08/03 : Speed up of MOS Model PSP

MOS Model PSP, level 100, is now 2 times faster than the previous version. The new version is available in SiMKit 2.2. More information about MOS Model PSP can be found here.

2005/04/11 : New models released: MOS Model PSP, level 100, and Juncap, level 200

MOS Model PSP, level 100, is now available. For more details on this model, see MOS Model PSP. Juncap, level 200, is also available now. For more details on this model, see Juncap.

2005/04/11 : SiMKit 2.1 released!

A new version of the SiMKit library is now available. SiMKit has been extended with MOS model PSP level 100, Juncap level 200, the bipolar model Modella level 500 including self-heating, and MOS model 20 level 2001 including self-heating.


Note that the release of the bipolar and the MOS model books, based on SiMKit 2.1, is delayed. The update of the models is described in reports that are available on this website.

2005/01/21 : Info available about relation between level and code version

An overview of the relation between the model level and the SiMKit code version has been added to the source code history of Bipolar Model Mextram 504 and MOS Model 11.
The background of the compact model identification is also described.


Note that the bipolar and the MOS model books, according to SiMKit 1.3, are now released.

2004/11/17 : SiMKit 2.0.1 released!

A new version of the SiMKit library is now available. SiMKit has been extended with Juncap level 1, the bipolar model Modella level 500, and MOS model 40 level 4000 including self-heating.

2004/11/17 : New Mextram publications and updates of Mextram and MOS reports

The reports of MOS Model Level 1100, Level 1101 and Level 1102 are updated. The report of the bipolar model Mextram, level 504, is updated. New publications about the bipolar model Mextram are added

2004/09/10 : Patch available for ADS SiMKit library

The official release of the ADS SiMKit library, version 1.3, contains a memory problem. A patch release can be obtained from Philips Send a message ED&T/Analogue Simulation support

2004/05/28 : SiMKit 1.3 released!

A new version of the SiMKit library is now available. SiMKit has been extended with self-heating for MOS11, level 1102.

2004/05/28 : Updates of Mextram and MOS reports

The reports of MOS Model Level 1100 and Level 1101 are updated.
The reports of the bipolar model Mextram, level 504, are updated.

2004/02/20 : SiMKit 1.2.1 released

A new version of the SiMKit library is now available. The release contains the new MOS models MM1102 and MM20.


Note that the releases of the bipolar and the MOS model books, related to SiMKit 1.2, are delayed. As soon as the model books will be released, they will be updated on this website. Descriptions of updates of recent models and descriptions of new models can be read in the model reports, see chapter 'additional reports' of all compact transistor models.

2004/02/20 : New MOS Model 11, level 1102, available!

MOS Model 11, level 1101, has been upgraded to MOS Model 11, level 1102. The main changes are:


  • Iterative solution of surface potential
  • More accurate, physics-based implementation of velocity saturation effect
  • More accurate, physics-based equations for thermal noise, induced gate noise and their correlation

More information, model equations and source code can be found here.

2004/02/20 : Test version of the new MOS Model 20 available!

The model equations and first source code of the new MOS Model 20 are now available. MOS Model 20 is a new compact model for an LDMOS transistor, which combines the MOSFET operation of the channel region with that of the drift region into one model. More information, model equations and source code can be found here.

2004/02/20 : Updates of Mextram and MOS reports

The reports of MOS Model Level 1100 and Level 1101 are updated.
The report of the bipolar model Mextram, level 504, is updated.

2003/12/07 : Update of SiMKit also available for ADS

A new version(1.1.1) of the SiMKit library is now available and is available for ADS as well.


Note that only the MOS models MM1100, MM1101 and MM3100 are available for this ADS SiMKit version.

2003/09/01 : The successor of PMK and SMK: SiMKit

SiMKit is a simulator-independent compact transistor model library. It is the successor of PMK and SMK. Simulator-specific connections are handled through so-called adapters that provide the right interfacing to Pstar and Spectre. The SiMKit library contains the most recent versions of the Philips transistor models.


Pstar

Using Pstar 4.5 or higher, the SiMKit library is set automatically by the Pstar cadenv. (Pstar 4.4 or lower, PMK is set automatically.)


Spectre

Depending on your Cadence version (4.4.6 or 5.0), you should install the right version of SiMKit. SiMKit is available for HPUX and SUNOS.

2003/06/13 : New documentation about Mextram and MOS1101 is available

The presentations “Modelling of Si and SiGe bipolar transistors with the compact model Mextram, level 504” and “Mextram (level 504). The Philips model for bipolar transistors” are available.


The report “physical background of MOS Model 11” is now available.

2003/01/13 : Update of SMK and PMK

New versions of the Spectre Modelkit (SMK 1.3) and the Pstar Modelkit (PMK 4.4) are now available. For Spectre, SMK is available for HPUX and SUNOS.


The updated libraries contain the most recent version of the bipolar model Mextram 504 and the most recent version of MOS model 1101.


For more details on these models, see Mextram or MOS Model 11.

2002/12/09 : Compact Transistor Models web-site renewed

In the renewed Compact Transistor Model web-site, the structure is organised in terms of the various models. In this way, only information about the model of interest is given which leads to more direct search results. The number of reports and publications that can be downloaded are increased giving more additional information. Further more, the model and source-code history can be observed in the "model & code history" page (examples: Mextram, MOS Model 11, MOS Model 40).

2002/05/14 : Philips models library for Spectre available!

The NXP compact models are available for Spectre. The models are included in a dynamic loaded library called SMK.


SMK 1.2 contains the most recent version of the bipolar model Mextram 504 and the most recent version of MOS model 1101.


For more details on these models, see Mextram or MOS Model 11.

2002/02/20 : New MOS Model, level 1101 available!

MOS Model 11, level 1100, has been upgraded to MOS Model 11, level 1101. The main changes are:

  • geometrical binning has been added
  • the physical geometry scaling rules have been improved
  • the temperature scaling has been brought from the level of maxiset (geometry independent parameters) to the level of miniset (geometry dependent parameters).

More information, model equations and source code can be found here.

2002/02/20 : Changes in MOS Model 11, level 1100

In MOS Model 11, level 1100, one constant has been changed. Details can be found in the preface of the document Download PDF File nlur2001_813.pdf (479kB).

2002/02/20 : Improvements and bug fixes to Mextram 504

A number of minor improvements and bug fixes have been added to Mextram 504:


  • non-self-heating and self-heating codes have been merged;
  • the behaviour of the external reverse diode has been improved;
  • all derivatives are now taken into account for the excess phase shift;
  • the minimum value for the thermal resistance has been put to zero;
  • the noise related to the non-constant part of the collector resistance has been corrected; and
  • the memory pointer error (reported by Texas Instruments) has been corrected.

More information, model equations and source code can be found here.

2001/05/01 : Source code of Mextram 504 with self-heating available!

The source code of the new Mextram 504 bipolar compact model including self-heating is now available. Moreover, Mextram 504 has been updated slightly by adding overlap capacitances. More information, model equations and source code can be found here.

2001/05/01 : Test version of the new MOS Model 11 available!

The model equations and first source code of the new MOS Model 11 are now available. MOS Model 11 is a surface-potential based compact MOS model that is completely symmetrical and offers a superior description of third-order harmonic distortion. Furthermore, it includes all relevant physical effects, e.g. gate leakage and quantum effects. More information, model equations and source code can be found here.

2001/03/01 : Report on parameter extraction of Mextram 504 available!

The source code of the new Mextram 504 bipolar compact model has been integrated in the Philips Modelkit and a report on the parameter extraction has become available (See the Additional reports section of Mextram). Four presentations on Mextram, which have been given at meetings of the Compact Model Council (see http://www.eigroup.org/cmc/) are now also available at this web site (see the Presentations about Mextram section). More information, model equations and source code can be found here.

2001/03/01 : Scaling rules MOS Level 903 extended

In new CMOS technologies the dopant concentration varies along the channel due to e.g. pocket implants. Consequently the mobility and thus the gain factor ßsq becomes a function of channel length. To take this effect into account the geometrical scaling rules of the gain factor, the threshold voltage, the drain-induced barrier-lowering and of the first mobility reduction parameter have been adapted. At the same time a quadratic term in the geometrical scaling rules of the body-effect factor has been added.

2001/03/01 : Improved accuracy and stability of MOS Model 31 & 40

While the model formulations and parameter sets remain unchanged, the implementation of both MOS Model 31 (level 3100) and 40 (level 40), the models for drain extensions of high-voltage MOS devices, have been improved for increased accuracy and numerical stability.

2001/03/01 : Report on parameter extraction and background of Modella

A report on the parameter extraction strategy and physical background of Modella, the compact model for lateral PNP bipolar transistors is now available (see the Additional reports section of Modella).

2000/07/17 : Test version of new Mextram 504 available!

The model equations and first source code of the much improved new Mextram 504 are now available. Mextram 504 has two main improvements with respect to Mextram 503: the description of the currents and charges is much smoother as function of bias and the parameter extraction has been improved. More information, model equations and source code can be found here.

1999/12/06 : New MOS Model 40 released

MOS Model 40, level 40, is a drain extension model for high-voltage MOS devices in SOI.

1999/12/06 : Update of MOS Model 31 released

The model equations of Model 31, level 3100, have been rewritten for improved numerical accuracy.

1999/12/06 : Update of MOS Model 903 released

Firstly, negative theta_3 values are not clipped to zero anymore, which improves the modelling of the saturation current of long-channel devices. Secondly, the maximum useful negative source-bulk voltage is increased to allow forward biasing of the junctions.

1999/12/06 : Rdiff model released

The Rdiff model is intended for modeling integrated semiconductor resistors. Source code is not available.

1998/11/23 : SI conversion of MOS Model 30

The equations of MOS Model 30 (level 3002), which is used for drain extensions in high-voltage MOS transistors, have been converted to SI units and are available as MOS Model 31, level 3100. The old model, MOS Model 3002, is still available.

1998/06/11 : New 1/f noise model in MOS Model 9, level 903

The new 1/f noise model in MOS Model 9, level 903, accounts for the bias dependence of the 1/f component of the input-referred noise. By setting the switch NFMOD equal to 1 the new 1/f noise model is activated, while NFMOD=0 (default) yields the level 902 noise model, in which the input-referred 1/f noise is bias independent. In this way parameter compatibility is maintained.


Note that in MOS Model 9, level 903, also the parameters WDOG and FTHE1 have been placed at their logical position in the parameter list.

1998/03/13 : New theta1 scaling rule in MOS Model 9

The theta1 scaling rule in MOS Model 9, level 902, has been modified to account for the effect of dogboning in narrow-width devices. The modelling accuracy for the linear and saturation currents has improved almost a factor of two! More information can be found in the documentation and in a recent publication.

1998/03/13 : New velocity saturation model in MOS Model 30

A new velocity saturation model has been implemented in MOS Model 30, level 3002, which is used for drain extensions in high-voltage MOS transistors. The monotonicity of the output characteristics has drastically improved!

1997/06/15 : Philips models available on world wide web!

All Philips compact models are now easily accessible on internet. The complete description of all model equations as well as the source code are available for downloading.

1997/06/15 : Change in the Juncap model

Note that in the present documentation the equation corresponding to Eq. (4.8) from Unclassified Report NL-UR 028/95 has changed.