Model history
Since the updates for SiMKit 3.1 (May 2008) the code history is included in the model history. Older code history can be found below.
Juncap level 200
Below is an overview of the relation between level and code versions. The background of the compact model identification scheme can be read here.
| Juncap 200 | SiMKit | ||
|---|---|---|---|
| level.version.implementation | code revision | release | date |
| 200.3.4 | 1.118.2.1 | 3.7 | 2011-08-04 |
| 200.3.4 | 1.109 | 3.6 | 2011-01-18 |
| 200.3.4 | 1.101 | 3.5.2 | 2010-10-12 |
| 200.3.4 | 1.84 | 3.4 | 2009-12-17 |
| 200.3.3 | 1.83 | 3.2, 3.3 | 2009/06/25 |
| 200.3.2 | 1.77 | 3.1.2 | 2008/07/24 |
| 200.3.1 | 1.76 | 3.1 | 2008/05/21 |
| 200.3.0 | 1.65.2.3 | 3.0.3 | 2008/01/31 |
| 200.2.1 | 1.49 | 2.5 | 2007/04/30 |
| 200.2.0 | 1.39 | 2.4 | 2006/10/23 |
| 200.1.2 | 1.27.2.1 | 2.3.2 | 2006/07/07 |
| 200.1.1 | 1.27 | 2.3 | 2006/03/16 |
| 200.1.0 | 1.23 | 2.2 | 2005/08/03 |
| 200.0.1 | 1.14 | 2.11 | 2005/04/11 |
| 2011/08 | Release of Juncap 200.3.4 |
| |
| 2010/10 | Release of Juncap 200.3.4 |
| |
| 2008/12 | Release of Juncap model, 200.3.3 |
| |
| 2008/05 | Release of Juncap model, 200.3.1 |
| minor code changes | |
| 2008/01 | Release of Juncap model, 200.3.0 |
| The newly introduced express-option of the JUNCAP2 model, invoked bysetting SWJUNEXP=1, allows the user to trade some simulation accuracyfor simulation speed. In transient analyses, a simulation time reductionof up to a factor of 5 (of the simulation time associated with JUNCAP2)has been demonstrated with a very limited loss of accuracy. This isachieved by a creating a strongly simplified IV-model, combined with amore extensive initialisation code. | |
| 2006/10 | Release of Juncap model, 200.2.0 |
| |
| 2005/08 | Release of Juncap model, 200.1.0 |
| 2005/03 | Release of Juncap model, 200.01.0, test version |
| 1988/10 | Introduction of the Juncap model, level 1. |
Juncap level 1
Below is an overview of the relation between level and code versions. The background of the compact model identification scheme can be read here.
| Juncap 1 | SiMKit | ||
|---|---|---|---|
| level.version.implementation | code revision | release | date |
| 1.1.7 | 1.130.2.1 | 3.7 | 2011-08-04 |
| 1.1.7 | 1.121.2.4 | 3.6 | 2011-01-18 |
| 1.1.6 | 1.110 | 3.5.2 | 2010-10-12 |
| 1.1.5 | 1.86 | 3.4 | 2009-12-17 |
| 1.1.4 | 1.84 | 3.3 | 2009/06/25 |
| 1.1.3 | 1.82.2.3 | 3.2 | 2008/07/24 |
| 1.1.2 | 1.80 | 3.1.2 | 2008/12/02 |
| 1.1.2 | 1.80 | 3.1 | 2008/05/21 |
| 1.1.1 | 1.77.2.1 | 3.0.3 | 2008/01/31 |
| 1.1.1 | 1.66 | 2.5 | 2007/04/30 |
| 1.1.0 | 1.59 | 2.4 | 2006/10/23 |
| 1.0.0 | 1.53 | 2.3 | 2006/03/16 |
| 2011/01 | Release of Juncap 1.1.7 |
| |
| 2010/10 | Release of Juncap 1.1.6 |
| Juncap has been implemented in a thread-safe way | |
| 2009/06 | Release of Juncap model,1.1.4 |
| Minor code changes | |
| 2008/12 | Release of Juncap model,1.1.3 |
| Extended the model with type parameter. The default for type is such that backwards compatibility is guaranteed. | |
| 1988/10 | Introduction of the Juncap model, level 1. |
Code history
Juncap level 200
The table below outlines the major changes to the file called "device_juncap2.c", which can be found in the source code.
| 2008/01/31 | Juncap model 200.3.0 |
| Code changes | |
| |
| 2007/04/30 | Juncap model 200.2.1 is identified in the code as revision 1.49. All code differences with the previous version (200.2.0) can be found in this diff file |
| Code changes | |
| |
| 2006/10/23 | Juncap model 200.2.0, which is identified in the code as revision 1.39. All code differences with the previous version (200.1.0) can be found in this diff file |
| Implemented Model changes | |
| |
| Other code changes | |
| None | |
| 2006/07/07 | Juncap model 200.1.2, which is identified in the code as revision 1.27.2.1. All code differences with the previous version (200.1.1) can be found in this diff file |
| Other code changes | |
| Some minor modifications | |
| 2006/03/16 | Juncap model 200.1.1, which is identified in the code as revision 1.27. All code differences with the previous version (200.1.0) can be found in this diff file |
| Implemented model changes | |
| Other code changes | |
| Some minor modifications | |
| 2005/08/03 | Juncap model 200.1.0, which is identified in the code as revision 1.23. All code differences with the previous version (200.0.1) can be found in this diff file |
| Implemented model changes | |
| Efficient limiting functions have been implemented | |
| Other code changes | |
| None | |
| 2005/04/11 | Juncap model 200.0.1 identified in the code as revision 1.14. |
| Release of Juncap model, level 200 |
Juncap level 1
The table below outlines the major changes to the file called "device_juncap.c", which can be found in the source code.
| 2007/04/30 | Juncap model 1.1.1 is identified in the code as revision 1.66. All code differences with the previous version (1.1.0) can be found in this diff file. |
| Code changes: | |
| |
| 2006/10/23 | Juncap model 1.1.0, which is identified in the code as revision 1.59. All code differences with the previous version (1.0.0) can be found in this diff file. |
|
Known bugs
There are no known bugs in the Juncap model.




Follow us