NXP fuels rise of mobile location-based services with ultra-low power, single-chip GPS solution
Recent acquisition quick to deliver best-in-class GPS technology within NXP’s mobile product portfolio
Quickly following the January 23rd closing of its acquisition of GPS technology provider GloNav, Inc., NXP Semiconductors today announced its first single-chip, Assisted-GPS (A-GPS) solution, designed for use in both mobile phones and standalone personal navigation devices (PNDs). Built on an advanced architecture, NXP's GNS7560 is the industry's smallest, lowest power, lowest system cost GPS solution.
To take these design advantages a step further, NXP has also integrated this best-in-class GPS technology into its existing Nexperia Cellular System Solution 7210 for 3G. This integration accelerates overall ease of use, system performance, time to market and cost effectiveness for mobile handset OEMs wanting to integrate powerful GPS capabilities in support of today's growing trend toward location-based services on mobile phones.
"NXP believes that location-based services are the next killer application in wireless, and our recent acquisition of GloNav is a testament to our belief in the endless possibilities that will arise with increased adoption of location-aware technologies," said Dennis Kish, Senior Vice President of Connected Entertainment, Business Unit Mobile & Personal at NXP Semiconductors. "We are excited that just two weeks after closing the transaction, the quick synergy between GloNav's technology and our existing product portfolio has allowed us to almost immediately offer our customers full access to an industry-leading GPS solution."
"Advances in GPS chipset development will significantly facilitate the low-cost integration of GPS technology with greater reliability and precision of satellite positioning in tomorrow's mobile devices, said Dominique Bonte, Principal Analyst, Telematics & Navigation at ABI Research. "By 2013, we can expect to see more than 900 million GPS-enabled devices in the market; each offering an array of new and innovative location-based services beyond traditional navigation, such as automatic geo-tagging of pictures taken with digital cameras, road toll systems, and social networking applications."
The NXP GNS7560 is implemented on a 90 nanometer (nm) architecture and features a high performance CMOS RF front end plus correlator engine to significantly reduce system cost and power. Advanced power management modes reduce power consumption to less than 13mW for one-second map updates – beyond any alternative GPS solution on the market today. With a package size of less than 9 mm2, the GNS7560 is the smallest GPS chip available, and when integrated with NXP's Cellular System Solution 7210, also provides the smallest overall solution.
Unlike other GPS solutions, the GNS7560 automatically alters sensitivity and tracking based on signal strength, multipath and velocity, delivering first-rate acquisition and tracking sensitivity, Time to First Fix (TTFF) and accuracy to ensure deep-indoor sensitivity and reliable coverage even in dense metropolitan areas known as 'urban canyons'. The host software for the product is structured for easy OS integration with Microsoft Windows® CE, Windows Mobile® and Linux standard drivers, as well as a variety of real-time kernels in support of today's Smartphone designs.
The high-performance GPS single-chip solution is integrated with NXP's Nexperia UMTS/EDGE Cellular System Solution 7210, which supports a broad set of multimedia applications and connectivity options for 2G and 3G mobile handsets. A demonstration of the Nexperia Cellular System Solution with integrated GNS7560 will be shown on NXP's booth (Hall 8, B110) at Mobile World Congress in Barcelona, Spain from February 11-14, 2008. .
Availablity
The standalone GNS7560 A-GPS solution is sampling now.
About NXP
NXP is a top 10 semiconductor company founded by Philips more than 50 years ago. Headquartered in Europe, the company has 37,000 employees working in more than 20 countries and posted sales of EUR 5 billion in 2006. NXP creates semiconductors, system solutions and software that deliver better sensory experiences in mobile phones, personal media players, TVs, set-top boxes, identification applications, cars and a wide range of other electronic devices. News from NXP is located at www.nxp.com.