Select site:
English
Product news
February 28, 2008

NXP Rides Wave of High FM Attach-rate in Mobile Devices



Eindhoven, The Netherlands, February 28, 2008 – Building on its leadership position in FM Radio ICs, NXP Semiconductors, the independent semiconductor company founded by Philips, today launched the world’s smallest highly-integrated FM stereo radio IC with R(B)DS functionality, the TEA5990. NXP's FM-RDS chip sets a new standard in radio performance, with better channel separation, best-in-class sensitivity, very high selectivity and clear sound. The TEA5990 inches ahead of competitive offerings by using a command-based interface to simplify software development, making system integration easy and quick to enable OEMs to drive higher attach rates for FM radio in portable devices.


Packaged in a 2.56x2.56mm size, the TEA5990 FM radio IC allows OEMs to implement a complete radio solution without external components requiring less than 15mm2 of board space. NXP’s FM-radio IC also enables quick integration and flexible design-ins by supporting the I2C-bus and the SPI-bus (3- or 4-wire format), while a digitally controlled algorithm facilitates seamless coexistence with GSM, Bluetooth, Wi-Fi and WiMAX. The TEA5990 also offers better reception quality over a wide tuning range (70 to 108 MHz, including the 70-MHz China band) with Stereo Noise Cancelling (SNC) as well as built-in Auto Search and Store for up to 32 channels with dynamic adjacent channel suppression.


“NXP’s TEA5990 helps manufacturers address the burgeoning demand for FM radio in low-cost handsets, by offering a low-cost solution that can be designed-in with complete ease,” said Timothy Wang, Marketing Manager for Connectivity and Broadcast Products, Mobile & Personal Business at NXP Semiconductors. “With consumers becoming more mobile globally, NXP’s chip with integrated RDS functionality makes it easier for users receive important announcements such as traffic updates, allowing any necessary journey changes to be made, while they listen to radio.”


“As the personal media player market grows to adopt FM functionality as a given standard, A-MAX is leveraging NXP’s TEA5990 FM-RDS chip to combine location-based service on PMPs,” said Frank Chang, General Manager for Marketing at A-MAX Technology. “With NXP’s TEA5990, A-MAX is poised to offer optimized production-ready reference designs to OEMs.”

 

Availability


NXP's FM-RDS stereo radio IC, TEA5990 will begin mass production end of Q1 2008, with a guide price of $1.00 for 100K quantities.

For more information on NXP’s TEA5990, click through here.

 

About NXP

NXP is a top 10 semiconductor company founded by Philips more than 50 years ago. Headquartered in Europe, the company has 37,000 employees working in more than 20 countries and posted sales of EUR 5 billion in 2006. NXP creates semiconductors, system solutions and software that deliver better sensory experiences in mobile phones, personal media players, TVs, set-top boxes, identification applications, cars and a wide range of other electronic devices. News from NXP is located at www.nxp.com.