NXP Semiconductors logo
Select site:
English
Product news
March 06, 2008

NXP Launches World’s Smallest Single-chip Triple-mode PCTV Solution


Brings revolutionary TV viewing experience to ultra-small form-factor portable computers and living room PCs


In a move to bring a high-quality anytime, anywhere TV viewing experience to ultra-mobile computers, NXP Semiconductors, the independent semiconductor company founded by Philips, today launched the world's smallest single-chip PCTV solution - SAA7231 - that supports worldwide broadcast standards. Packaged in half the size of a minicard, NXP's latest innovation is 40 percent power-efficient, saves OEMs up to 15 percent of total BOM (bill-of-materials) cost, and speeds up time-to-market under one month.

 

NXP's SAA7231 is ideally suited for TV cards in current and future flavors of Microsoft Media Centre Edition (MCE) PCs, with support for analog, DVB-T and DVB-S broadcasts as well as an integrated MCE-compliant IR controller for a full-function remote control. A state-of-the-art video processing engine decodes the analog AV stream for features such as PVR and time shifting, while adaptive 2D noise reduction improves picture quality. The SAA7231 also includes certified three-level Macrovision® detection circuitry to keep the video's original analog copy protection intact.

 

“The proliferation of ultra-mobile computers and the desire for staying tuned to live TV broadcasts is necessitating the adoption of ultra-small universal PCTV solutions, such as NXP's SAA7231,” said Martin Maloney, Marketing Director for PC Systems, Home business unit, NXP Semiconductors. “The small size, low-cost, low-power, high-level of integration and maturity of NXP's PCTV solution will enable manufacturers to offer high-quality TV viewing as a standard feature in portable computers, full-featured desktops and living room PCs.”

 

NXP's SAA7231 can be packaged into 10mmx10mm size with support for PCI / PCIe interfaces and is capable of consuming as little as 1.5Watts of power to ensure uninterrupted streaming of AV content with extended playback time. The SAA7231 is also supported by a device driver package for Microsoft's BDA (Broadcast Driver Architecture) for Windows Vista and XP.

 

Availability

The world's smallest single-chip triple mode PCTV solution, SAA7231, from NXP is on demo at CeBIT 2008 in Hannover, Germany from 4–9 March.

 

For more information on NXP’s latest PCTV solution, SAA7231, click here.

 

About NXP Semiconductors

NXP is a top 10 semiconductor company founded by Philips more than 50 years ago. Headquartered in Europe, the company has 37,000 employees working in more than 20 countries and posted sales of USD 6.3 billion in 2007. NXP creates semiconductors, system solutions and software that deliver better sensory experiences in mobile phones, personal media players, TVs, set-top boxes, identification applications, cars and a wide range of other electronic devices. News from NXP is located at www.nxp.com.