Select site:
English
Product news
June 05, 2008

NXP First To Deliver NorDig-compliant System-Level STB Solution


Enables OEMs to offer best-in-class digital reception, picture and sound quality, speed-up time-to-market


Eindhoven, The Netherlands, June 05, 2008 - NXP Semiconductors, the independent semiconductor company founded by Philips, today announced that its STB100 T21 reference board is the first full digital terrestrial system-level solution to have passed the NorDig 1.0.3 verification test process. The NorDig 1.0.3 compliance will ensure that the STB100 reference board is capable of spectacular digital reception and offers OEMs a simple, well-designed, affordable set-top box solution. For consumers, NXP's validated STB100 will, in turn, deliver superior picture and sound quality on mainstream set-top-boxes.


NXP's STB100 T21 reference board incorporates the highly integrated silicon tuner TDA18211, state-of-the-art channel decoder for digital terrestrial reception - TDA10048, and the Nexperia MPEG source decoder, PNX8300 - all of which combined fulfill the RF performance requirements under the NorDig Unified Specification 1.0.3. tested and verified in Teracom's laboratory in Sweden. Ideal for mainstream free-to-air or pay television, the STB100 is a dedicated solution for single-channel digital STB ‘Zapper Boxes’ and iDTV systems.


“As the transition from analog to digital TV broadcasting gains momentum around the world, NXP is delivering solutions to power enhanced viewing experiences across the complete spectrum of set-top box and digital TV applications,” said Menno Kleingeld, senior director and general manager for vertical STB business at NXP Semiconductors. “Being the first to achieve NorDig-compliance at the system-level for STB100 reiterates NXP's commitment to deliver reliable, production-ready solutions to our customers and partners.”


During the NorDig 1.0.3 RF conformance tests conducted by Teracom, NXP's STB100 T21 reference board proved to be a well-designed, stable and reliable system-level solution delivering high-quality digital reception. The stringent standards enforced through NorDig-compliance enable manufacturers to address mainstream set-top box market demand quickly and cost-effectively, no matter which geography they are in.


Key features of NXP's STB100 T21 reference board include:


  • A low-power, 24-bit stereo audio DAC
  • On-board front panel (LED + IR receiver)
  • RGB, CVBS and S-video outputs
  • Optional smart card mounting
  • External or internal power supply
  • Customized remote control
  • SPDIF digital audio output

For more information on NXP's STB100, click here.


About NXP Semiconductors

NXP is a top 10 semiconductor company founded by Philips more than 50 years ago. Headquartered in Europe, the company has 37,000 employees working in more than 20 countries and posted sales of USD 6.3 billion in 2007. NXP creates semiconductors, system solutions and software that deliver better sensory experiences in mobile phones, personal media players, TVs, set-top boxes, identification applications, cars and a wide range of other electronic devices. News from NXP is located at www.nxp.com.