NXP Semiconductors logo
Select site:
English
Product news
Press image
August 27, 2008

NXP enhances next-generation Digital Recording+ on new Loewe LCD TVs with SAA7164 System-On-Chip


Highly integrated SAA7164 SoC offers 3D comb-filtering and noise reduction


Eindhoven, The Netherlands, August 27, 2008 – NXP Semiconductors, the independent semiconductor company founded by Philips, today announced that Loewe, a leading European TV manufacturer, has chosen its SAA7164 system-on-chip to add Digital Video Recorder (DVR) and Time Shifting functionality to its new hybrid LCD TV models. The SAA7164 is used as the core SoC of a highly integrated encoder module that enables consumers to pause or record analog sources in addition to digital programs onto a hard disk drive (HDD), without the need for an external set-top box (STB). The advanced 3D comb-filtering and noise reduction offered by the SAA7164 offers optimal video quality of all recorded material. The new hybrid LCD TV models from Loewe will be showcased at IFA in Berlin, Germany from August 29 to September 3, 2008.

 

“As HD LCD TVs offer increased functionality, it’s ideal for Loewe to add features such as digital recording and time-shifted playback that ensure the same picture quality level from recorded as well as live content on our new hybrid LCD TV models,” said Dr. Uwe Bach, head of TV development at Loewe. “The SAA7164 solution from NXP will allow our customers to record and watch all types of analog sources such as movies or their favorite TV shows at any time, pause live TV or skip within time-shift recorded content without the need for an additional STB.”

 

“Loewe’s choice of the SAA7164 system-on-chip with advanced 3D comb-filtering and noise reduction is in line with Loewe and NXP’s ambition to offer more content with the highest possible picture quality on television sets, whether it is broadcast or recorded,” said Rolf-Dieter Gutsmann, product marketing manager, TV systems, NXP Semiconductors.

 

The NXP SAA7164 integrates up to 8 standalone chips: two IF demodulators, two PAL/NTSC/SECAM decoders, two stereo decoders, plus two multi-format compression engines.

 

More information on the NXP SAA7164 is available at: Integrated solution for DVR and time shifting in Consumer Electronics.applications.

 

 

Loewe TVs with SAA7164 at IFA

The new TV models of Loewe, featuring the NXP SAA7164 will be presented in the Loewe booth (number 201, hall 6.2b) at IFA in Berlin from August 29 to September 3.

 

About NXP Semiconductors

NXP is a leading semiconductor company founded by Philips more than 50 years ago. Headquartered in Europe, the company has 31,000 employees working in more than 20 countries and posted sales of USD 6.3 billion (including the Mobile & Personal business) in 2007. NXP creates semiconductors, system solutions and software that deliver better sensory experiences in TVs, set-top boxes, identification applications, mobile phones, cars and a wide range of other electronic devices. News from NXP is located at www.nxp.com.