NXP Delivers Highest RF Output Power for L-band Radar Applications
New device based on Generation 6 LDMOS technology delivers more than 50% efficiency with unprecedented ruggedness
Eindhoven, Netherlands, November 20, 2008 – Expanding its portfolio of industry-leading RF power transistors, NXP Semiconductors, the independent semiconductor company founded by Philips, today launched its latest Laterally Diffused Metal Oxide Semiconductor (LDMOS) transistor for L-band radar applications delivering breakthrough RF output power of 500W at frequencies between 1.2GHz and 1.4GHz.
Targeted at a wide range of L-band radar applications, NXP’s LDMOS L-band RF power transistor sets new standards for efficiency (>50 percent drain efficiency), gain (17dB) and ruggedness at 500W power level when compared to competing bipolar.
“As the first company that launched LDMOS for L- and S-band applications, NXP’s high-efficiency LDMOS RF power transistor portfolio is establishing a new industry standard by providing our customers with the ultimate performing and most rugged transistor available on the market,” said Mark Murphy, international product marketing manager, RF power products, NXP Semiconductors. “The breakthrough in RF output power of 500W is the result of NXP’s collaborative approach with customers, which helped us to deliver easy to design-in transistors for quick time-to-market.”
Key performance parameters for NXP’s L-band RF transistor (BLL6H1214-500), include:
- 500W peak output power (at 1.4GHz, 100µs pulse width, 25 percent duty cycle)
- 17dB gain
- 50 percent drain efficiency
- Improved ruggedness
- Overdrive without risk up to 5dB
- Improved pulse droop (0.2dB)
- Supply Voltage 50V
- Non-toxic packaging and ROHS compliance
NXP’s device combines the power density of bipolar with the advantages of LDMOS technology for L- band Radar design, and allows for a replacement of the BeO containing packages by an environmentally friendly ceramic package.
Availability
NXP’s BLL6H1214-500 LDMOS L-band RF power transistor is available immediately. More information on NXP’s BLL6H1214-500 is available at http://www.nxp.com/pip/BLL6H1214-500_PL_1.html
For NXP’s wide range of industry leading 6th generation LDMOS technology. For more information click through http://www.nxp.com/campaigns/experience_rfpower
About NXP Semiconductors
NXP is a leading semiconductor company founded by Philips more than 50 years ago. Headquartered in Europe, the company has about 33,500 employees working in more than 20 countries and posted sales of USD 6.3 billion (including the Mobile & Personal business) in 2007. NXP creates semiconductors, system solutions and software that deliver better sensory experiences in TVs, set-top boxes, identification applications, mobile phones, cars and a wide range of other electronic devices. News from NXP is located at www.nxp.com.