NXP Semiconductors logo
Select site:
English
Product news
October 08, 2008

NXP Makes High-Power Stereo Sound More Affordable


Launches world’s first 2x170W integrated stereo class-D amplifier for use on single layer PCBs


NXP Semiconductors, the independent semiconductor company founded by Philips, today launched the industry’s first highly integrated stereo class-D amplifier suitable for single layer PCB use, TDA8950 – delivering bigger, better sound on slim-line audio systems. NXP’s TDA8950, a 2x150W to 170W class-D amplifier, has been specially designed for use on single-layer PCBs – feeding into manufacturer demand for more power with smaller design and lower costs.

 

NXP’s TDA8950 supports audiophile audio performance with very low dissipation, operates over a wide supply voltage range from ±12.5V to ±40V and consumes a very low quiescent current. Combined with improved EMI performance and thermal fold-back to avoid audio stops, the TDA8950 offers significant performance and cost efficiencies to enable OEMs to deliver high-power stereo output with sleek design – including, mini / micro Hi-Fi’s, home theatre systems, professional music amplifiers and public address systems.

 

“NXP’s TDA8950 stereo class-D amplifier is a perfect fit for futuristic slim-line audio systems. As consumers demand high-quality performance at competitive prices, the ability to use a single layer PCB allows significant savings in cost, while the TDA8950 delivers excellent audio.”

 

Jan-Paul Huyser, international product marketing manager for audio amplifier ICs at NXP Semiconductors, said: “Building on our leadership position in audio amplifiers, NXP’s TDA8950 mirrors market demand and provides customers a complete amplification module to aid their development of advanced audio solutions, enhancing performance while reducing time to market.”

 

Key features of NXP’s TDA8950 integrated stereo class-D amplifier include:

  • Fully integrated stereo SE class-D amplifier
  • Up to 2x170W output power
  • Integrated Pulse Width Modulation (PWM) controller with 2nd order feedback
  • 85V total maximum operating supply voltage
  • Excellent audio with low distortion levels
  • Up to 10dB improvement in EMI radiation levels
  • Thermal fold-back with a tiny heat sink ensure uninterrupted audio performance at high IC temperatures
  • Pop free on/off switching
  • High power supply noise rejection ratio
  • Current clipping protection (will not switch off when a complex speaker load forces the over- current protection to be activated)

 

Availability

The 2x170W integrated stereo class-D amplifier for use on single layer PCBs from NXP – TDA8950 is available now and in mass production from September 2008.

 

For more information on NXP’s TDA8950 stereo class-D amplifiers, click through http://www.nxp.com/acrobat_download/datasheets/TDA8950_1.pdf

 

About NXP Semiconductors

NXP is a leading semiconductor company founded by Philips more than 50 years ago. Headquartered in Europe, the company has about 33,500 employees working in more than 20 countries and posted sales of USD 6.3 billion (including the Mobile & Personal business) in 2007. NXP creates semiconductors, system solutions and software that deliver better sensory experiences in TVs, set-top boxes, identification applications, mobile phones, cars and a wide range of other electronic devices. News from NXP is located at www.nxp.com.