NXP Semiconductors logo
Select site:
English
Product news
Press image
July 08, 2009

NXP Claims Breakthrough in MOSFET Performance with World’s First Sub 1 MilliOhm MOSFET in a Power S08 Package


World First From NXP Sets New Efficiency Standards for MOSFET Performance


Eindhoven, the Netherlands, July 8, 2009 – NXP Semiconductors, the independent semiconductor company founded by Philips, today announced the world’s first n-channel sub 1 milliOhm 25V MOSFET, PSMN1R2-25YL , boasting the lowest ever RDSon and best in class Figure of Merit. This is the lowest ever RDSon MOSFET in a Power-SO8 package (Loss Free package: LFPAK) and is an extension to NXP’s existing MOSFET portfolio. The newest generation MOSFET combines the high performance Power-S08 LFPAK package with latest Trench 6 generation silicon and offers numerous performance and reliability advantages in a wide variety of demanding applications such as: power OR-ring, motor control and high efficiency synchronous buck-regulators.

 

“The technology for producing MOSFETs is an ongoing race to improve performance,” says John David Hughes, Senior International Product Marketing Manager of NXP. “We are using innovative techniques in the new Trench 6 process which further reduce the on-resistance. There are many advantages of the new Trench technology to our customers such as improved switching efficiency from the silicon and superior electrical and thermal resistance from the package. NXP’s Power-S08 (LFPAK) package is compatible with all widely accepted Power SO-8 PCB footprints.”

 

NXP’s world leading Trench 6 MOSFETs, PSMN1R2–25YL, has a typical RDSon of 0.9 mOhm for a 25V part in Power-S08 (LFPAK), and 1.0 mOhm (typical) for a 30V part.

 

In addition to launch of the world’s lowest RDSon MOSFET, NXP is announcing a new portfolio of products aimed at power supply, motion control, and industrial markets. The range includes products with operating voltages of 25, 30, 40 and 80 volts, packaged in Power-S08 (LFPAK) and TO220.

 

Availability

PSMN1R2–25YL is now available at $0.80 (for 1000 pieces).

For datasheets and more information about NXP’s new Trench 6 MOSFETs, please visit: http://www.nxp.com/infocus/topics/lowest_rds_mosfet/index.html

 

About NXP Semiconductors

NXP is a leading semiconductor company founded by Philips more than 50 years ago. Headquartered in Europe, the company has about 28,000 employees working in more than 30 countries and posted sales of USD 5.4 billion (including the Mobile & Personal business) in 2008. NXP creates semiconductors, system solutions and software that deliver better sensory experiences in TVs, set-top boxes, identification applications, mobile phones, cars and a wide range of other electronic devices. News from NXP is located at www.nxp.com.