Select site:
English
Business News From Philips Semiconductors
August 27, 2001

Philips Semiconductors and Streaming Networks introduce real-time consumer MPEG-4 video encoder



Sunnyvale, Calif., August 27, 2001- Philips Semiconductors, a division of Royal Philips Electronics (NYSE:PHG, AEX:PHI), today announced that Streaming Networks will provide a real-time consumer MPEG-4 video-encoder targeted for its Trimedia™ very long instruction word (VLIW) media processor. This partnership provides a one-chip solution ideally suited for embedded applications such as security systems, surveillance systems, video streaming and video on demand.


The MPEG 4 encoder is capable of producing bit streams that are fully compliant with MPEG-4 ISO/IEC 14496-2 Simple Visual Profile and Main Visual Profile. The rate controller is tuned for optimum performance for bit rates ranging from 384 Kbits per second up to 4 Mbits per second. Among other features, the encoder is able to generate error resilient video streams, and supports concurrent encoding of multiple rectangular video objects in real time. Additionally, the encoder supports both progressive and interlaced videos and compression tools.


"The combination of Streaming Networks expertise in MPEG 4 and Philips Semiconductors TriMedia VLIW media processor technology will enable our customers to bring a new generation of products to market quickly," said Ayub Khan, president, Streaming Networks. "This combination of the TriMedia VLIW media processor and MPEG 4 video encoder is a key element for any internet appliance or streaming video solution."


"Together, Philips Semiconductors and Streaming Networks, are delivering a one-chip solution capable of MPEG-4 video encoding and decoding," said Eric Freid, business development manager, business line media processing, Philips Semiconductors. "Our continuing relationship with Streaming Networks and other partners will provide our customers with a complete one-chip solution, giving them a market advantage by streamlining their development process."


Philips Semiconductors will be demonstrating its leadership in TriMedia VLIW and MPEG 4 at IFA 2001 from August 27th through August 31st.

About Streaming Networks

Streaming Networks is a leader in the design and development of embedded multimedia solutions. Streaming Networks provides quality multimedia software, ranging from libraries and applications to complete system solutions, for the expanding multimedia and communications markets. In its portfolio, it has high quality, highly optimized ISO/ITU compliant video encoders (MPEG1, MPEG4, H.263 and H.261) and ISO/ITU compliant audio multi-channel encoders/decoders (AAC, G.711, G.722, G.723, G.728 and G.729a). We also offer system integration services and TriMedia based reference design for hosted and standalone development. This one stop shop approach allows our customers to explore new technology horizons for their next generation products. For more information: www.streaming-networks.com.

About Philips Semiconductors

Philips Semiconductors, with revenues of US $6.3 billion in 2000, is a world leader in silicon systems and standard products for wireless communications, digital entertainment, computing and automotive applications. The organization designs, develops and manufactures silicon solutions based on its innovative Nexperia™ architecture to create living technology for its customers building products, service providers using the products, and consumers enjoying the resulting products and services. For more information: www.semiconductors.philips.com.

Note
TriMedia is a media processing technology wholly-owned by TriMedia Technologies Inc
TriMedia is a trademark of TriMedia Technologies Inc.