NXP Semiconductors logo
Select site:
English
Product News From Philips Semiconductors
February 11, 2002

Philips Semiconductors reinvents radio architecture


Integrated FM-Stereo broadcast receiver chips bring radio to portable consumer devices


Philips Semiconductors, a division of Royal Philips Electronics (NYSE: PHG, AEX: PHI), has made a breakthrough with the launch of a family of fully-integrated single chip stereo radios for low voltage and low power applications. Making significant cuts in the number of external components and the cost of the peripherals, the radio is completely adjustment free and can tune into European, US and Japanese FM bands. With the growing demand to integrate radios into mobile phones, this new development will transcend current industry capabilities, allowing radios to feature in a variety of portable devices where there is little space available. The first chips to be released will be the TEA5767 and the TEA5768.

Despite changing lifestyles, the popularity of radio continues. To enable equipment manufacturers to capitalize on this demand, Philips Semiconductors has pioneered its new architectural approach. Designers will now be able to incorporate the radio function into a variety of consumer devices including mobile phones, MP3 players, portable CD players, toys and promotional giveaways. The simplicity of design-in and small chip size of the new family will help in furthering the proliferation of radios in portable hand-held devices.


"Philips Semiconductors has realised a breakthrough in radio architecture design in such a way that expensive external parts have been replaced by smart silicon. This has resulted in lower material costs and a smaller footprint for the total radio function, giving simpler radio design. The latter translates into faster time to market for our customers," commented Kees Joosse, market sector team manager at Philips Semiconductors. "Capitalizing on the trend for access to radio at any time, in any place, this new family of chips will enable the inclusion of radios in a whole new set of products. 'One-chip radio' is now becoming a reality, which will enable many new, exciting innovations."


Classical radio architecture requires external parts to be aligned during production. Many of these external parts handle high frequency signals, which need very carefully-designed Printed Circuit Boards (PCBs). The TEA5767 and TEA5768 chips have much fewer external parts than standard chips. They need no alignments and PCB design is much less complicated because of the small footprint of the total radio function when using the new chip.


Samples of TEA5767 and TEA5768 are currently available. Volume production will begin in the first quarter of 2002.


About Philips Semiconductors


Philips Semiconductors, a top ten semiconductor supplier with revenues of US $4.4 billion in 2001, is a world leader in silicon systems and standard products for consumer, communications, automotive and computing products. The organization designs, develops and manufactures silicon solutions based on its innovative Nexperia™ architectures to create living technology for its customers creating products, service providers using the products, and consumers enjoying the resulting products and services. For more information: www.semiconductors.philips.com