Underscoring our market leadership in car entertainment, we recently shipped our 50 millionth car radio / audio DSP, the SAF7730. With the SAF7730, a member of the Dirana family, we are a key supplier to the large majority of car radio set makers and car manufacturers worldwide.
The SAF7730 is a dual IF car radio / audio DSP that offers excellent radio and audio quality by using multiple integrated cores and leading software features such as phase diversity. Its software-defined architecture enables customers to differentiate their products while reducing development costs and shortening time-to-market. By launching new software releases on a regular basis, NXP continues to update the SAF 7730 with new and improved features and functions. The SAF7730 is sold as a chipset solution with up to two tuner front-end ICs (the TEF6721 and the TEF6730).
The recently introduced SAF7741 follows on the success of the SAF7730. The SAF7741, which combines with the tuner front-end IC TEF7000, delivers a low-IF architecture to the high-performance car OEM market. It raises the performance bar for modern car radios while slashing the costs for external components count and reducing board space by almost 50%.
NXP also offers the SAF7746, a dedicated, single-tuner version of the Dirana family.
Regular updates
To keep current with our latest announcements, be sure to sign up for eNews, our customizable electronic newsletter that saves you time by sending you only the information you want.




Follow us