MediaTek chooses NXP BISS-Technology

January 05, 2011
SOT1118

MediaTek chooses NXP BISS-Technology New integrated solution reduces footprint by 50%

MediaTek Inc. the leading fabless semiconductor company for wireless communications and digital multimedia solutions has added NXP to its approved vendor list: The use of a NXP low saturation voltage "BISS" transistor and a small-signal MOSFET for the battery charger unit of its mobile platform MT6236 has already been confirmed.

Additionally, a new solution by NXP integrating these two products in the leadless, ultra thin 2 x 2 mm SMD package SOT1118 is currently under test at MediaTek. This solution is reducing the footprint by more than 50% and at the same time lowering the package height from 1 down to 0.65 mm. A significant step towards miniaturization of the PCB.

Schematic diagram

MediaTek approved NXP BISS / MOSFET solution Integrated solution in a SOT1118 package (under test at MediaTek)
Schematic Diagram Schematic Diagram
PBSS5350D
  • 50 V, 3 A bipolar low VCEsat PNP transistor
  • In a 6-pin SOT457 (2.8 x 2.9 x 1 mm)
PBSM5240PF
  • 40 V, 2 A bipolar low VCEsat PNP transistor
  • Integrated 30 V N-channel MOSFET
  • In a 6-pin leadless SOT1118 (2 x 2 x 0.65 mm)
PMR400UN
  • 30 V N-channel MOSFET
  • In a 3-pin SOT416 (1.6 x 0.8 x 0.5 mm)
 
PMZ390UN
  • 30 V N-channel MOSFET
  • In a 3-pin leadless SOT883 (1 x 0.6 x 0.5 mm)
 

Footprint Reduction

Related links

Further information about the new low saturation "BISS" transistor / MOSFET solution is available from NXP MarCom

Regular updates

To keep current with our latest announcements, be sure to sign up for eNews, our customizable electronic newsletter that saves you time by sending you only the information you want.

How to search?