NXP first to offer one silicon platform for digital and analog HD LCD TVs for all consumer markets globally

September 04, 2006

Nexperia TV520/507 reference designs offer unprecedented efficiency, speed and cost advantages for TV manufacturers

Eindhoven, The Netherlands, 4th September 2006 – NXP, the newly independent semiconductor company founded by Philips, today announced two new TV reference designs: Nexperia™ TV520/32 for DVB/PAL and Nexperia TV507 for analog TVs. Both reference designs are based on one global silicon platform that enables TV manufacturers to develop hybrid digital and analog LCD TV sets with best-in-class picture quality and unique design-in benefits.


With the TV520/32 for DVB/PAL and the earlier introduced TV520/30 and TV520/20 for ATSC, NXP is now able to offer one hybrid platform for all regions worldwide. The TV507 is based on the same platform and offers the analog-only version, thus enabling NXP’s customers to spin off an analog-only product from the same platform investment. All members of the family are pin-to-pin compatible, which means TV designers can re-use the investments across a range of products.


Set makers profit from reduced development costs, easy design-in processes and shorter lead times. With its unique features, the TV520 platform allows NXP’s customers to develop a product and bring it to market in as little as three months. Consumers benefit from having a uniform user interface for analog as well as digital channels. Furthermore, it enables a new, brilliant viewing experience as best–in-class picture quality can be offered at an affordable price point.


"Our solution is unique as it is based on one silicon platform serving the two worlds of digital and analog TV sets. It is cost-effective and efficient for manufacturers to only work with one platform and offer two different end products with high picture quality," said Jos Klippert, marketing director, Digital TV solutions, NXP. "As more High Definition TV content becomes available, consumers are seeking LCD TVs that offer the highest quality analog as well as digital viewing experience at an affordable price."


The TV520 reference design is built on the Nexperia Home media processor, which provides the IP blocks for MPEG de-multiplexing and decoding, video scaling, de-interlacing, noise reduction, all kinds of video featuring, video rendering, audio decoding, digital-to-analog conversion and audio featuring. It also contains a High Definition Multimedia Interface (HDMI) and an SD/HD analog component input. The TV520 reference design is also scalable to higher-end TV solutions by simply adding a variety of NXP’s companion processors.


Availability

The reference design will be available in Europe and APAC in Q1, 2007.


About NXP:

NXP is a top 10 semiconductor company founded by Philips more than 50 years ago. Headquartered in Europe, the company has 37,000 employees working in 20 countries across the world. NXP creates semiconductors, system solutions and software that deliver better sensory experiences in mobile phones, personal media players, TVs, set-top boxes, identification applications, cars and a wide range of other electronic devices. News from NXP is located at www.nxp.com.

Nexperia is a trademark of NXP.


Forward-looking Statements

This release may contain certain forward-looking statements with respect to the financial condition, results of operations and business of NXP and certain plans and objectives of NXP with respect to these items. By their nature, forward-looking statements involve risk and uncertainty because they relate to events and depend on circumstances that will occur in the future and there are many factors that could cause actual results and developments to differ materially from those expressed or implied by these forward-looking statements.

How to search?