NXP delivers ultra-thin EMI filters with highest integrated ESD protection

March 21, 2007

Breakthrough EMI filters in UTLP feature integrated ESD protection of ±30 kV

NXP, the independent semiconductor company founded by Philips, today announced breakthrough EMI filters featuring the industry’s highest level of ESD protection – ±30-kV contact – available in NXP’s award-winning ultra-thin leadless package (UTLP). With a height of only 0.5 mm and a pad pitch of 0.4 mm, the IP4253 and IP4254 are also among the thinnest EMI filters available on the market today.  The ultra-thin, ultra-robust electromagnetic interference filters are designed for portable applications such as mobile phones, PDAs, MP3 players and GPS navigators featuring ultra-slim designs.
 

“Thin handsets are ‘in’ – and they will continue to become thinner – as consumers embrace the fashion, portability and longer battery life of ultra-slim mobile devices,” said Frans Scheper, general manager, general application discretes business line, and senior vice president, NXP Semiconductors.  “With the NXP IP4253 and IP4254 series in UTLP, handset manufacturers can take advantage of the ultra-compact EMI filters which vastly reduce the size of the PCB and double the level of integrated ESD protection available for their thinnest handset designs. For consumers, this means more brilliant displays and higher sound quality on the slimmest and most stylish handsets.”
 

Solving EMI and ESD for a more vibrant mobile multimedia experience
With so much functionality available in mobile multimedia devices – from radio, Bluetooth and MP3 music playback to high-resolution LCD displays, video cameras and TV-on-mobile – the RF transceiver in the handset interferes with more interfaces, making a higher degree of EMI filtering essential. Further, the core ICs in mobile multimedia devices also require a higher level of protection from electrostatic discharge, since they are manufactured using smaller process technologies to enable a higher level of integration. By delivering high-quality EMI filtering with the industry’s highest ESD protection – ±30-kV contact, or twice the level previously available – the NXP IP4253 and IP4254 EMI filters address a critical need in the market today.
 

Innovation in ultra-thin design
The NXP IP4253 and IP4254 series of EMI filters in UTLP offer a 90-percent space reduction compared to alternative discrete technology.  With a pad pitch of only 0.4 mm, the IP4253 and IP4254 in UTLP enable a space reduction of more than 30 percent compared to alternative solutions in a 0.5-mm pitch size.  
 

The breakthrough in ultra-thin EMI filters is enabled by the UTLP platform developed by NXP. The NXP UTLP platform – winner of the 2006 Hong Kong Award for Industries: Technological Achievement Award – gives designers the flexibility to add more functionality into smaller spaces in consumer electronics products, through a patent-pending substrate and etching technology. UTLP increases the “silicon to plastic” ratio and offers less parasitic capacitance and inductance compared to other plastic packages, due to shorter wire length and internal traces, making it ideally suited for high-frequency applications.
 

Other NXP products currently available in UTLP include the IP4221CZ6-XS ESD protection chip, which features a record 0.35-mm pitch.
 

Availability
The IP4253 and IP4254 EMI filters in UTLP are available immediately in 4-, 6- and 8-channel configurations, each with component values of 15 pF – 100 ? - 15 pF and 15 pF – 200 ? - 15 pF. Production quantities are fully available in a fully RoHS compliant, lead-free version, as well as a green package version without halogens in the plastic.  Further information is available at: http://www.nxp.com/products/discretes/esd_emi_filtering/.
 

Additional information on NXP’s comprehensive portfolio of ultra-small leadless devices in SOD882/SOT883 (sized 1.0 x 0.6 x 0.5 mm), is available at: http://www.nxp.com/products/discretes/.

 

About NXP

NXP is a top 10 semiconductor company founded by Philips more than 50 years ago. Headquartered in Europe, the company has 37,000 employees working in 26 countries across the world. NXP creates semiconductors, system solutions and software that deliver better sensory experiences in mobile phones, personal media players, TVs, set-top boxes, identification applications, cars and a wide range of other electronic devices. News from NXP is located at http://www.nxp.com/.

How to search?