Continuing to deliver the technology behind the mobile lifestyle, NXP Semiconductors, the independent semiconductor company founded by Philips, today announced the availability of its complete WiMAX 2x2 MIMO (Multiple Input Multiple Output)-powered family of transceivers for mobile and handheld applications. In support of the mass deployment of mobile WiMAX, NXP’s new family of transceivers employ 2x2 MIMO technology, allowing for twice the data throughput and double the maximum speed of the company’s existing WiMAX transceiver solutions. NXP’s transceiver solutions will allow WiMAX infrastructure OEMs and ODMs to implement more robust WiMAX functionality, while achieving unparalleled savings in overall power, board real-estate and system costs.
“Imagine being able to watch interactive TV combined with graphic rich gaming on the move, or even having a multi-person video chat while accessing the internet or reading email. WiMAX is a key enabler in this vibrant portable media environment,” said Marcel van Roosmalen, general manager RF WiMAX product line, NXP Semiconductors. “Through its design innovation and strong partnerships in the WiMAX ecosystem, NXP is delivering on the promise of mobile WiMAX to offer users low cost access to broadband communication anytime, anywhere.”
One of few 2x2 MIMO WiMAX solutions in the industry, NXP’s new family of UXA234xx WiMAX transceivers improves reach and drives greater bandwidth and spectral efficiency, being particularly effective for accessing a WiMAX connection in dense urban areas. Further, because 2x2 MIMO allows for dual input and output channels, it addresses the requirements of bandwidth-intensive mobile applications, such as streaming data, voice and video data, without compromising network load and at a much lower cost to carriers. End users can thus experience speeds of up to 15 MB – three to five times faster than today's wireless broadband cellular networks.
“WiMAX is changing the way and speed that consumers will access content by permitting a quadruple play of voice, video and data transfer while on-the-move, allowing the connected consumer to engage in a truly nomadic way of life” said Will Strauss, analyst, Forward Concepts. “MIMO-powered WiMAX is significant because it delivers higher bandwidth at less cost.”
In addition, building on the success of NXP’s first family of WiMAX transceivers, the new family guarantees seamless handover from base station to base station – one of the biggest challenges facing designers of WiMAX equipment. The new family also delivers optimum interoperability with a variety of basebands by utilizing standard analog I/Q and serial interfacing, and co-exists with cellular, WLAN and Bluetooth standards.
The UXA234XX WiMAX transceivers offer a fully integrated direct-up transmitter and ZIF architecture with a small foot print of 6x6x0.85mm. The solution set supports channel bandwidths from 3.5 MHz - 20 MHz and various flexible calibration techniques for optimum performance and lowest power consumption. With no need for an external IF filter, the solution set requires minimum external components.
Availability
The UXA23466 and UXA23476 WiMAX 2x2 MIMO transceivers are sampling now. Volume production will start in Q2. To view a live demonstration of NXP’s WiMAX MIMO solutions, visit the NXP Booth #1803 at CTIA Wireless in Orlando, Florida from March 27-29, 2007.
About NXP WiMAX Solutions
NXP offers a comprehensive solution for the emerging WiMAX standard in both base stations and handsets. The NXP UXA234xx series is a set of fully integrated, low-power, direct conversion transceivers, which enable easy, robust and reliable broadband communication for mobile devices such as phones, PCMCIA cards, laptops and PDAs. Featuring ultra-low noise, high dynamic range and high linearity, the UXA234xx transceivers allow seamless handover between base stations. NXP has been a member of the WiMAX Forum since January 2006.
About NXP
NXP is a top 10 semiconductor company founded by Philips more than 50 years ago. Headquartered in Europe, the company has 37,000 employees working in 26 countries across the world. NXP creates semiconductors, system solutions and software that deliver better sensory experiences in mobile phones, personal media players, TVs, set-top boxes, identification applications, cars and a wide range of other electronic devices. News from NXP is located at www.nxp.com.




Follow us