NXP and Siemens develop GPS/GSM-based toll system for private vehicles

May 06, 2008

Breakthrough telematics solution enables cost-effective, simple installation and enforcement

Eindhoven, The Netherlands, 6 May, 2008 - NXP and Siemens Mobility have reached an agreement to technically collaborate with each other in order to develop NXP's new ATOP (Automotive Telematics On Board Unit Platform) into the 'single chip on-board unit' system based on GPS and GSM. Once it is ready for the market, it is intended for use in private vehicles. ATOP can be used simply and cost-effectively as it exploits existing GPS/GSM mobile networks. It is not necessary to install expensive infrastructure such as toll stations. Drivers can install the on-board unit for private cars in just a few minutes. The system is secure and facilitates easy toll collection. Commercial use is planned for the first half of 2010.


Governments, authorities and institutions all over the world are becoming increasingly interested in flexible road pricing solutions that are suitable for all car drivers and can automatically calculate and charge customers for a journey by car. In addition, they must not impair the flow of traffic and must help to ensure that the number of vehicles on the roads is kept within reasonable limits. Siemens Mobility and NXP are therefore working together to create a viable, practical solution for the market. NXP will supply a chip and basic software which combines all the functions for toll collection such as GPS (Global Positioning System), GPRS (General Packet Radio Service) and NFC (Near Field Communication) modules. Interfaces for flexible telematics applications such as additional traffic information, including the Smart X high-safety application, will be provided on a single-chip platform, which is fully automotive-grade. Siemens is to develop the on-board unit (OBU) and integrate the single chip and software from NXP.


The previous toll system from Siemens Mobility will thus be considerably improved on in terms of the range of functions. The ATOP-based on-board unit receives GPS satellite signals and uses GSM-based standard radio technology for transmitting data to the central system for toll calculation. The system also includes a non-removable adhesive vignette which is fitted with a radio chip (RFID) and is attached to the windscreen. It communicates with the on-board unit in order to ensure that the OBU is actually present in the vehicle and is being operated in accordance with the use for which it is intended. The RFID vignette can also be used for other applications such as parking space management.


The price of a car journey can be determined in a number of ways. The distance traveled and the time of day chosen for the trip are the main factors, but the type of vehicle and fuel consumption or CO2 emissions are also possible references. Simple, secure toll charging is ensured by means of monthly invoicing but, in order to ensure privacy, a prepaid card can be purchased instead. In this case, no details of the driver or the route are disclosed.


The current fee for car journeys can be displayed by the OBU at all times. The police or authorized monitoring bodies can carry out a check at any time to make sure the driver is using the system in the way for which it is intended, enabling easy enforcement. For this purpose, a portable device will be provided which uses near field communication technology (NFC) in order to read out information from the vignette on the windscreen. The vignette also serves as a security mechanism in conjunction with the OBU in order to ensure than only the OBU specifically assigned to the vehicle can be used and not exchanged with another vehicle.


The OBU is being developed to take into account the conditions inside the vehicle. This is necessary in order to enable it to withstand extreme temperatures. The lifetime of the unit is not dependent on the lifetime of the vehicle. The system is being developed in such a way that it can be easily fitted in the vehicle and, in the event of damage, can easily be replaced.


Further information on intelligent traffic systems from Siemens Mobility at http://www.siemens.de/traffic.

About NXP

NXP is a top 10 semiconductor company founded by Philips more than 50 years ago. Headquartered in Europe, the company has 37,000 employees working in more than 20 countries and posted sales of USD 6.3 billion in 2007. NXP creates semiconductors, system solutions and software that deliver better sensory experiences in mobile phones, personal media players, TVs, set-top boxes, identification applications, cars and a wide range of other electronic devices. News from NXP is located at www.nxp.com.


About Siemens

The Siemens Industry Sector (Erlangen, Germany) is the worldwide leading supplier of production, transportation and building technologies. With integrated hardware and software technologies as well as comprehensive Industry-specific solutions, Siemens increases the productivity and efficiency of its customers in the fields of industry and infrastructure. The Sector consists of six divisions: Building Technologies, Industry Automation, Industry Solutions, Mobility, Drive Technologies and OSRAM. With around 209,000 employees worldwide Siemens Industry achieved in fiscal 2007 total sales of approximately EUR40 billion (pro forma, unconsolidated). www.siemens.com/industry


The Siemens Mobility Division (Erlangen, Germany) is the internationally leading provider of transportation and logistics solutions. With its "Complete Mobility" approach, the Division is focused on networking the various modes of transportation in order to ensure the efficient transport of people and goods. Complete Mobility combines the company's competence in operations control systems for railways and traffic control systems for roadways together with solutions for airport logistics, postal automation, traction power supplies and rolling stock for mass transit, regional and mainline services, as well as forward-looking service concepts.

How to search?