NXP real-time clock sets new record in power efficiency

June 10, 2008

PCF2123 real-time clock features tiny foot print and delivers extremely long stand-by time in handheld devices

Eindhoven, Netherlands, June 10, 2008 - Today, NXP Semiconductors, the independent company founded by Philips, announced the availability of the industry's best low-power performance real-time clock (RTC) chips with SPI bus interface, the PCF2123. Operating at a current of less than 100 NanoAmperes (0.15uW) on a 1.5-V power supply, the real-time clock comes in a tiny 3x3x1mm package, making it ideal for battery operation and handheld applications to keep track of time, when the equipment is powered down. The small size and low-power requirement of the PCF2123 make it a good choice for applications including home-use medical devices such as blood pressure monitors, portable phones, PDAs and similar compact portable electronics products where space and power are critical, while the variety of features makes it suitable for industrial systems as well as white goods.


“Power consumption is probably the most important feature of RTCs, directly correlated to the battery life of the electronic equipment,” said Markus Hintermann, international product manager, interface product line, NXP Semiconductors. “Three parameters are very critically watched during system design including accuracy, power consumption and size. Using precision engineering, NXP has been able to develop a groundbreaking real-time clock that can save 50 percent or more power.”


Features of the PCF2123 real-time-clock include a freely programmable alarm and timer function that gives designers the option to generate a wake-up signal on an interrupt pin. A programmable offset register also allows fine-tuning of the clock and frequency adjustment. The seconds, minutes, hours, days, weekdays, months and years registers are all coded in binary-coded decimal (BCD) format for easy conversion to decimal digits for printing or display and faster decimal calculations. Data is transferred serially via an SPI bus with a maximum data rate of 6.25 Mbits per second.


Accuracy on the real-time clock is maintained by using a quartz reference. Each of these CMOS-based, real-time clock/calendars uses a low-power 32.768-kHz quartz oscillator to provide clock and calendar functions. The calendar functions track year, month, date, and day with built-in century and leap-year flags. The tolerance of the quartz and the physical environment around the quartz crystal and oscillator circuit can be easily calibrated via the on-chip calibration register. No other external parts are required.


Real-time clocks are indispensable for time keeping, process control and other time-critical tasks found in time-keeping applications, battery-powered stand-by devices, and in metering units. The PCF2123 is a CMOS real-time clock and calendar optimized for low power consumption. It functions as the time manager accurately keeping time, controlling the periodic wake-up of the microcontroller core from hibernation mode, and providing a watchdog function to independently monitor microcontroller tasks. With power consumption at less than 0.15uW the RTC can be powered by a very small battery cell or a small super-cap. Housed in tiny 3x3x1mm leadless package, the RTC fits nearly anywhere minimizing the space needed to host this important timing and measurement function.


Pricing and Availability

Samples of the PCF2123 real-time clocks are available now. Volume shipping begins in Q2 2008.


About NXP Semiconductors

NXP is a top 10 semiconductor company founded by Philips more than 50 years ago. Headquartered in Europe, the company has 37,000 employees working in more than 20 countries and posted sales of USD 6.3 billion in 2007. NXP creates semiconductors, system solutions and software that deliver better sensory experiences in mobile phones, personal media players, TVs, set-top boxes, identification applications, cars and a wide range of other electronic devices. News from NXP is located at www.nxp.com.

How to search?