Eindhoven, The Netherlands - NXP Semiconductors, the independent semiconductor company founded by Philips, has launched an innovative new web-based design and monitoring solution for power management ICs. To help designers keep development time as short as possible, the tool provides comprehensive online design support and technology to create a one-stop shop for the full design cycle.
The online tool is an easy to use, accessible web browser-based configuration application to drive efficiency in the design process. NXP’s PIP8000 power-supply interface allows power supplies to be monitored, configured and sequenced in order to create a multi-purpose design environment. NXP customers can also use the tool to customize their design requirements virtually, significantly reducing development time. As well as real-time feedback facilities and diagnostics, the web tool offers the freedom to configure a power system in-line with PMBus command language and physical interface.
“We are the first in the industry to release this new online design tool as our customers are demanding significantly improved online services. It helps to keep development cycles as short as possible. In our efforts to support the complete design cycle, this is a great step forward” said Michel Claassens, Head of Global Brand Experience NXP Semiconductors.
The online design tool can be used to control and monitor the power management application. Using a wide range of PMBus commands the user can quickly adjust voltage and current settings, control fan speed and monitor the power management system’s thermal behaviour as well as logging power system parameters. This enables the user to add full range of control option, including power sequencing, to an existing analog power solution.
"NXP's PIP8000 is a powerful PMBus compliant power management supervisor IC," stated Edwin Kluter, Marketing Director of Power Solutions, NXP Semiconductors. "The new PIP8000 online interface further shows our commitment to providing our customers with leading online design support and technology. With the PMBus web design tool, our customers will be able to customize their design requirements virtually to significantly reduce the design time required."
Online design tool capabilities include:
- Configurable GUI, (simulating PMBus host) which automatically locates all connected devices with verified NXP PIP8000 defaults
-
PMBus scripting and debug capabilities
-
Compliant to PMBus 1.1 command set
-
Support of linear and direct mode data formats, switched in real time
-
User commands and graph viewing includes: voltage, current, fans, and thermals
-
Fan controls allow switch-on/switch-off of up to two fans, as well as reading the fan speeds in RPM
The tool can be found on the NXP website: http://web.transim.com
About NXP Semiconductors
NXP is a leading semiconductor company founded by Philips more than 50 years ago. Headquartered in Europe, the company has about 28,000 employees working in more than 30 countries and posted sales of USD 5.4 billion (including the Mobile & Personal business) in 2008. NXP creates semiconductors, system solutions and software that deliver better sensory experiences in TVs, set-top boxes, identification applications, mobile phones, cars and a wide range of other electronic devices. News from NXP is located at www.nxp.com.




Follow us