NXP Dual Tuner RF System Brings Integration Breakthrough to Satellite Set-top Boxes

August 10, 2009

NXP TDA20136 features unprecedented levels of pre-tuner RF functionality, supporting single cable and legacy satellite reception

NXP, the independent semiconductor company founded by Philips, today unveiled its latest silicon tuner innovation with the industry’s most highly integrated dual-stream RF system for both single cable and legacy satellite reception. The new NXP TDA20136 integrates a dual 8PSK satellite tuner with an unrivaled level of pre-tuner circuitry to create a single platform that delivers the flexibility to be used in diverse installation scenarios without any hardware changes, while dramatically reducing design cost and complexity.

The pre-tuner circuitry provides the flexibility that allows set-top boxes to be used in dissimilar installation scenarios - either with a single cable input, splitting the signal internally to the device, or in legacy mode with two separated inputs. In both cases, an optional dual loopthrough function is available.

The most common use case for the single input setting is when the set-top box is used with a Single Cable Reception outdoor unit (ODU). In this case, signals from multiple Low Noise Blocks (LNBs) are multiplexed onto a single cable at the ODU. This single cable can then provide the required signals for many set top boxes in a single home or multi-dwelling unit (MDU). With no hardware changes, a set-top box using this IC can also be used in an installation with a legacy multi-LNB, multi-cable ODU. In this legacy installation, each tuner gets its signal from a separate cable.

“The industry trend towards Single Cable Reception has the potential to dramatically reduce installation costs because there are fewer cables to install, but implementing SCR circuitry in a set-top box using a standard satellite tuner is complex and expensive,” said Tim Kirstein, NXP Semiconductors. “We have created the TDA20136 with the highest levels of RF integration to directly address these problems, while also providing the set-top box maker with the flexibility to be backwards compatible with traditional multi-LNB, multi-cable ODUs.”

The TDA20136 system is based on NXP’s proven superior-performance dual-tuner technology, the CX24132. This unique second-generation complete dual 8PSK tuner offers outstanding performance and low power consumption. It includes all necessary Low Noise Amplifiers (LNAs), Voltage-Controlled Oscillators (VCOs), synthesizers, mixers and filters required for common applications, and its small (7mm x 7mm) size allows system designers to reduce the size of front-ends.

Availability

The NXP TDA20136 will be available globally and will be in production from September 2009. For more information about NXP’s RF silicon tuners, please visit:http://www.nxp.com/products/rf/tuners/silicon_tuners

About NXP Semiconductors

NXP is a leading semiconductor company founded by Philips more than 50 years ago. Headquartered in Europe, the company has about 29,000 employees working in more than 30 countries and posted sales of USD 5.4 billion (including the Mobile & Personal business) in 2008. NXP creates semiconductors, system solutions and software that deliver better sensory experiences in TVs, set-top boxes, identification applications, mobile phones, cars and a wide range of other electronic devices. News from NXP is located at www.nxp.com.

How to search?